4.1.8.3 Net Socket Service

The Net Socket service provides network and socket services to the user application. It includes DHCP server configuration for the Wi-Fi® interface and API's for socket operations such as open, read, write and close. It also provides 2 simultaneous TLS configuration instances which can be used with a given socket communication tunnel. The Net service API call syntax is provided below:
SYS_WINCS_RESULT_t SYS_WINCS_NET_SockSrvCtrl( SYS_WINCS_NET_SOCK_SERVICE_t request, SYS_WINCS_NET_HANDLE_t netHandle);
Figure 4-34. Net System Service Configuration in MCC

This section allows NET service basic configuration as mentioned below:

  • Number of Sockets: Configure this field in the range of 1-2.
  • Mode: Server/Client Mode Selection
  • Ip Protocol: TCP/UDP protocol selection.
  • IP Type : Select IP type : IPv4 / IPv6 Local / IPv6 Global.
  • Server address: Enter the respective server IP address.
  • Socket Port: Socket port number.
  • Enable TLS: Select to enable TLS Configuration option.
    • Peer authentication
      • Root CA / Server Certificate
    • Device Certificate
    • Device Key
    • Device Key Password
    • Server Name
    • Domain Name Verify
      • Domain Name
Note: Update the SYS_WINCS_NET_NO_OF_CLIENT_SOCKETS macro in sys_wincs_net_service.h to reflect the number of client sockets the system can manage in server mode. (supports max 5 clients).

The Net service provides the following services for the user:

Net Socket Services

Services/OptionsInput ParametersDescription
SYS_WINCS_NET_TLS_CONFIGSYS_WINCS_NET_TLS_SOC_PARAMS structureUse the TLS configuration
SYS_WINCS_NET_DHCP_SERVER_ENABLEDHCP Configuration: Set IP, Pool startEnable the DHCP server
SYS_WINCS_NET_DHCP_SERVER_DISABLENoneDisable the DHCP server
SYS_WINCS_NET_SOCK_TCP_OPENSYS_WINCS_NET_SOCKET_t strucutureOpen TCP socket. Returns socket ID.
SYS_WINCS_NET_SOCK_UDP_OPENSYS_WINCS_NET_SOCKET_t strucutureOpen UDP socket. Returns socket ID.
SYS_WINCS_NET_SOCK_CLOSESocket IDClose the socket
SYS_WINCS_NET_SOCK_SET_CALLBACKCallback function handlerRegister application callback for socket
SYS_WINCS_NET_SOCK_SET_SRVC_CALLBACKDHCP Callback function handlerRegister application callback for socket
SYS_WINCS_NET_SOCK_GET_CALLBACKCallback Function HandlerGet callback information
SYS_WINCS_NET_OPEN_TLS_CTXNULLOpen TLS Handle
SYS_WINCS_NET_GET_TLS_CTX_HANDLEempty TLS handleGet TLS Handle

The events that are returned in the Net socket service are provided below:

Table 4-6. Net Sock Events List
EventsResponse ComponentsDescription
SYS_WINCS_NET_SOCK_EVENT_CONNECTEDNULLReports the socket connected event
SYS_WINCS_NET_SOCK_EVENT_TLS_DONENULLTLS handshake done, on this event the TLS configuration instance can be re used for other TLS sessions
SYS_WINCS_NET_SOCK_EVENT_READSocket ID (Integer)

Length (Integer)

Reports the length of data available on the given socket ID
SYS_WINCS_NET_SOCK_EVENT_UNDEFINEDNoneSocket Undefined Event
SYS_WINCS_NET_SOCK_EVENT_CLIENT_CONNECTEDSocket ID (Integer)Client Connected Event
SYS_WINCS_NET_SOCK_EVENT_ERRORSocket ID (Integer)

Error code(Integer)

Reports the socket error events
SYS_WINCS_NET_SOCK_EVENT_CLOSEDSocket ID (Integer)Disconnects to Socket

The basic net socket service sequence chart is provided below:

Figure 4-35. Basic Net Socket Service Sequence Chart

Socket Write

The socket service provides the write API for the TCP and UDP sockets. Following are the API prototypes:
SYS_WINCS_RESULT_t SYS_WINCS_NET_TcpSockWrite( uint32_t socket, uint16_t length, uint8_t *input);
SYS_WINCS_RESULT_t SYS_WINCS_NET_UdpSockWrite( uint32_t socket, uint8_t *addr, uint32_t port, uint16_t length, uint8_t *input);
Socket Read

The socket service provides the read API for the TCP and UDP sockets. Following are the API prototypes:

int16_t SYS_WINCS_NET_TcpSockRead( uint32_t socket, uint16_t length, uint8_t *input);
int16_t SYS_WINCS_NET_UdpSockRead( uint32_t socket, uint16_t length, uint8_t *input);

The sample TCP socket example is provided below:

Some of the configurations can be configured by MCC.
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdlib.h>
#include <time.h>
#include "configuration.h"
#include "driver/driver_common.h"

#include "app_wincs02.h"
#include "system/system_module.h"
#include "system/console/sys_console.h"
#include "system/wifi/sys_wincs_wifi_service.h"
#include "system/sys_wincs_system_service.h"
#include "system/net/sys_wincs_net_service.h"

// *****************************************************************************
// *****************************************************************************
// Section: Global Data Definitions
// *****************************************************************************
// *****************************************************************************

// *****************************************************************************
/* Application Data

  Summary:
    Holds application data

  Description:
    This structure holds the application's data.

  Remarks:
    This structure should be initialized by the APP_Initialize function.

    Application strings and buffers are be defined outside this structure.
*/

APP_DATA g_appData;


// Define and initialize a TCP client socket configuration from MCC
SYS_WINCS_NET_SOCKET_t g_tcpClientSocket = {
    // Specify the type of binding for the socket
    .bindType = SYS_WINCS_NET_BIND_TYPE0,
    // Set the socket address to the predefined server address
    .sockAddr = SYS_WINCS_NET_SOCK_SERVER_ADDR0,
    // Define the type of socket (e.g., TCP, UDP)
    .sockType = SYS_WINCS_NET_SOCK_TYPE0,
    // Set the port number for the socket
    .sockPort = SYS_WINCS_NET_SOCK_PORT0,
    // Enable or disable TLS for the socket
    .tlsEnable = SYS_WINCS_TLS_ENABLE0,
    // Specify the IP type (e.g., IPv4, IPv6)
    .ipType  = SYS_WINCS_NET_SOCK_TYPE_IPv4_0,
};

// *****************************************************************************
// *****************************************************************************
// Section: Application Callback Functions
// *****************************************************************************
// *****************************************************************************


/* TODO:  Add any necessary callback functions.
*/

// *****************************************************************************
// Application NET Socket Callback Handler
//
// Summary:
//    Handles NET socket events.
//
// Description:
//    This function handles various NET socket events and performs appropriate actions.
//
// Parameters:
//    socket - The socket identifier
//    event - The type of socket event
//    netHandle - Additional data or message associated with the event
//
// Returns:
//    None.
//
// Remarks:
//    None.
// *****************************************************************************
void SYS_WINCS_NET_SockCallbackHandler
(
    uint32_t socket,                    // The socket identifier
    SYS_WINCS_NET_SOCK_EVENT_t event,   // The type of socket event
    SYS_WINCS_NET_HANDLE_t netHandle    // Additional data or message associated with the event
) 
{
    if(socket == g_tcpClientSocket.sockID)
    {
        switch(event)
        {
            /* Net socket connected event code*/
            case SYS_WINCS_NET_SOCK_EVENT_CONNECTED:    
            {
                SYS_CONSOLE_PRINT(TERM_GREEN"[APP] : Connected to Server!\r\n"TERM_RESET );
                break;
            }

            /* Net socket disconnected event code*/
            case SYS_WINCS_NET_SOCK_EVENT_DISCONNECTED:
            {
                SYS_CONSOLE_PRINT(TERM_RED"[APP] : Socket DisConnected!\r\n"TERM_RESET);
                SYS_WINCS_NET_SockSrvCtrl(SYS_WINCS_NET_SOCK_CLOSE, &socket);
                break;
            }

            /* Net socket error event code*/
            case SYS_WINCS_NET_SOCK_EVENT_ERROR:
            {
                SYS_CONSOLE_PRINT(TERM_RED"[APP ERROR] : Socket Error\r\n"TERM_RESET);
                break;
            }

            /* Net socket read event code*/
            case SYS_WINCS_NET_SOCK_EVENT_READ:
            {         
                uint8_t rx_data[64];
                int16_t rcvd_len = 64;
                memset(rx_data,0,64);

                // Read data from the TCP socket
                if((rcvd_len = SYS_WINCS_NET_TcpSockRead(socket, SYS_WINCS_NET_SOCK_RCV_BUF_SIZE, rx_data)) > 0)
                {
                    rcvd_len = strlen((char *)rx_data);
                    rx_data[rcvd_len] = '\n';
                    SYS_CONSOLE_PRINT(TERM_YELLOW"Received ->%s\r\n"TERM_RESET, rx_data);

                    // Write the received data back to the TCP socket
                    if (SYS_WINCS_FAIL == SYS_WINCS_NET_TcpSockWrite(socket, rcvd_len, rx_data))
                    {
                        g_appData.state = APP_STATE_WINCS_ERROR;
                    }
                }    
                break;
            }
            case SYS_WINCS_NET_SOCK_EVENT_CLOSED:
            {
                SYS_CONSOLE_PRINT(TERM_RED"[APP] : Socket CLOSED -> socketID: %d\r\n"TERM_RESET,socket);
                break;
            }

            case SYS_WINCS_NET_SOCK_EVENT_TLS_DONE:    
            {
                SYS_CONSOLE_PRINT("[APP] : TLS ->Connected to Server!\r\n" );
                break;
            }

            default:
                break;                  
        }   
    }
    /* TODO:  Add if conditions for any more sockets.
    */
}



// *****************************************************************************
// Application Wi-Fi Callback Handler
//
// Summary:
//    Handles Wi-Fi events.
//
// Description:
//    This function handles various Wi-Fi events and performs appropriate actions.
//
// Parameters:
//    event - The type of Wi-Fi event
//    wifiHandle - Handle to the Wi-Fi event data
//
// Returns:
//    None.
//
// Remarks:
//    None.
// *****************************************************************************
void SYS_WINCS_WIFI_CallbackHandler
(
    SYS_WINCS_WIFI_EVENT_t event,         // The type of Wi-Fi event
    SYS_WINCS_WIFI_HANDLE_t wifiHandle    // Handle to the Wi-Fi event data
)
{

    switch(event)
    {
        /* Set regulatory domain Acknowledgment */
        case SYS_WINCS_WIFI_REG_DOMAIN_SET_ACK:
        {
            // The driver generates this event callback twice, hence the if condition 
            // to ignore one more callback. This will be resolved in the next release.
            static bool domainFlag = false;
            if( domainFlag == false)
            {
                SYS_CONSOLE_PRINT("Set Reg Domain -> SUCCESS\r\n");
                g_appData.state = APP_STATE_WINCS_SET_WIFI_PARAMS;
                domainFlag = true;
            }
            
            break;
        } 
        
        /* SNTP UP event code*/
        case SYS_WINCS_WIFI_SNTP_UP:
        {            
            SYS_CONSOLE_PRINT("[APP] : SNTP UP \r\n"); 
            break;
        }
        break;

        /* Wi-Fi connected event code*/
        case SYS_WINCS_WIFI_CONNECTED:
        {
            SYS_CONSOLE_PRINT(TERM_GREEN"[APP] : Wi-Fi Connected    \r\n"TERM_RESET);
            break;
        }
        
        /* Wi-Fi disconnected event code*/
        case SYS_WINCS_WIFI_DISCONNECTED:
        {
            SYS_CONSOLE_PRINT(TERM_RED"[APP] : Wi-Fi Disconnected\nReconnecting... \r\n"TERM_RESET);
            SYS_WINCS_WIFI_SrvCtrl(SYS_WINCS_WIFI_STA_CONNECT, NULL);
            break;
        }
        
        /* Wi-Fi DHCP IPv4 complete event code*/
        case SYS_WINCS_WIFI_DHCP_IPV4_COMPLETE:
        {         
            SYS_CONSOLE_PRINT("[APP] : DHCP IPv4 : %s\r\n", (char *)wifiHandle);
            
            g_appData.state = APP_STATE_WINCS_CREATE_SOCKET;
            break;
        }
        
        case SYS_WINCS_WIFI_DHCP_IPV6_LOCAL_COMPLETE:
        {
            //SYS_CONSOLE_PRINT("[APP] : DHCP IPv6 Local : %s\r\n", (char *)wifiHandle);
            break;
        }
        
        case SYS_WINCS_WIFI_DHCP_IPV6_GLOBAL_COMPLETE:
        {
            //SYS_CONSOLE_PRINT("[APP] : DHCP IPv6 Global: %s\r\n", (char *)wifiHandle);
            break;
        }
        
        default:
        {
            break;
        }
    }    
}


// *****************************************************************************
// *****************************************************************************
// Section: Application Local Functions
// *****************************************************************************
// *****************************************************************************


/* TODO:  Add any necessary local functions.
*/


// *****************************************************************************
// *****************************************************************************
// Section: Application Initialization and State Machine Functions
// *****************************************************************************
// *****************************************************************************

/********************************************************************************/

// *****************************************************************************
// Application Initialization Function
//
// Summary:
//    Initializes the application.
//
// Description:
//    This function initializes the application's state machine and other
//    parameters.
//
// Parameters:
//    None.
//
// Returns:
//    None.
//
// Remarks:
//    None.
// *****************************************************************************

 
void APP_WINCS02_Initialize ( void )
{
    // Place the App state machine in its initial state. */
    g_appData.state = APP_STATE_WINCS_PRINT;



    /* TODO: Initialize your application's state machine and other
     * parameters.
     */
}


// *****************************************************************************
// Application Tasks Function
//
// Summary:
//    Executes the application's tasks.
//
// Description:
//    This function implements the application's state machine and performs
//    the necessary actions based on the current state.
//
// Parameters:
//    None.
//
// Returns:
//    None.
//
// Remarks:
//    None.
// *****************************************************************************

void APP_WINCS02_Tasks ( void )
{
    /* Check the application's current state. */
    switch ( g_appData.state )
    {
        // State to print Message 
        case APP_STATE_WINCS_PRINT:
        {
            SYS_CONSOLE_PRINT(TERM_YELLOW"########################################\r\n"TERM_RESET);
            SYS_CONSOLE_PRINT(TERM_CYAN"        WINCS02 TCP Client demo\r\n"TERM_RESET);
            SYS_CONSOLE_PRINT(TERM_YELLOW"########################################\r\n"TERM_RESET);
            
            g_appData.state = APP_STATE_WINCS_INIT;
            break;
        }
        
        /* Application's initial state. */
        case APP_STATE_WINCS_INIT:
        {
            SYS_STATUS status;
            // Get the driver status
            SYS_WINCS_WIFI_SrvCtrl(SYS_WINCS_WIFI_GET_DRV_STATUS, &status);

            // If the driver is ready, move to the next state
            if (SYS_STATUS_READY == status)
            {
                g_appData.state = APP_STATE_WINCS_OPEN_DRIVER;
            }

            break;
        }

        case APP_STATE_WINCS_OPEN_DRIVER:
        {
            DRV_HANDLE wdrvHandle = DRV_HANDLE_INVALID;
            // Open the Wi-Fi driver
            if (SYS_WINCS_FAIL == SYS_WINCS_WIFI_SrvCtrl(SYS_WINCS_WIFI_OPEN_DRIVER, &wdrvHandle))
            {
                g_appData.state = APP_STATE_WINCS_ERROR;
                break;
            }

            // Get the driver handle
            SYS_WINCS_WIFI_SrvCtrl(SYS_WINCS_WIFI_GET_DRV_HANDLE, &wdrvHandle);
            g_appData.state = APP_STATE_WINCS_DEVICE_INFO;
            break;
        }

        case APP_STATE_WINCS_DEVICE_INFO:
        {
            APP_DRIVER_VERSION_INFO drvVersion;
            APP_FIRMWARE_VERSION_INFO fwVersion;
            APP_DEVICE_INFO devInfo;
            SYS_WINCS_RESULT_t status = SYS_WINCS_BUSY;

            // Get the firmware version
            status = SYS_WINCS_SYSTEM_SrvCtrl(SYS_WINCS_SYSTEM_SW_REV, &fwVersion);

            if(status == SYS_WINCS_PASS)
            {
                // Get the device information
                status = SYS_WINCS_SYSTEM_SrvCtrl(SYS_WINCS_SYSTEM_DEV_INFO, &devInfo);
            }

            if(status == SYS_WINCS_PASS)
            {
                // Get the driver version
                status = SYS_WINCS_SYSTEM_SrvCtrl(SYS_WINCS_SYSTEM_DRIVER_VER, &drvVersion);
            }

            if(status == SYS_WINCS_PASS)
            {
                char buff[30];
                // Print device information
                SYS_CONSOLE_PRINT("WINC: Device ID = %08x\r\n", devInfo.id);
                for (int i = 0; i < devInfo.numImages; i++)
                {
                    SYS_CONSOLE_PRINT("%d: Seq No = %08x, Version = %08x, Source Address = %08x\r\n", 
                            i, devInfo.image[i].seqNum, devInfo.image[i].version, devInfo.image[i].srcAddr);
                }

                // Print firmware version
                SYS_CONSOLE_PRINT(TERM_CYAN "Firmware Version: %d.%d.%d ", fwVersion.version.major,
                        fwVersion.version.minor, fwVersion.version.patch);
                strftime(buff, sizeof(buff), "%X %b %d %Y", localtime((time_t*)&fwVersion.build.timeUTC));
                SYS_CONSOLE_PRINT(" [%s]\r\n", buff);

                // Print driver version
                SYS_CONSOLE_PRINT("Driver Version: %d.%d.%d\r\n"TERM_RESET, drvVersion.version.major, 
                        drvVersion.version.minor, drvVersion.version.patch);
                
                g_appData.state = APP_STATE_WINCS_SET_REG_DOMAIN;
            }
            break;
        }

        case APP_STATE_WINCS_SET_REG_DOMAIN:
        {
            // Set the callback handler for Wi-Fi events
            SYS_WINCS_WIFI_SrvCtrl(SYS_WINCS_WIFI_SET_CALLBACK, SYS_WINCS_WIFI_CallbackHandler);

            SYS_CONSOLE_PRINT(TERM_YELLOW"[APP] : Setting REG domain to " TERM_UL "%s\r\n"TERM_RESET ,SYS_WINCS_WIFI_COUNTRYCODE);
            // Set the regulatory domain
            if (SYS_WINCS_FAIL == SYS_WINCS_WIFI_SrvCtrl(SYS_WINCS_WIFI_SET_REG_DOMAIN, SYS_WINCS_WIFI_COUNTRYCODE))
            {
                g_appData.state = APP_STATE_WINCS_ERROR;
                break;
            }
            g_appData.state = APP_STATE_WINCS_SERVICE_TASKS;
            break;
        }

        case APP_STATE_WINCS_SET_WIFI_PARAMS:
        {
            // Configuration parameters for Wi-Fi station mode
            SYS_WINCS_WIFI_PARAM_t wifi_sta_cfg = {
                .mode        = SYS_WINCS_WIFI_MODE_STA,        // Set Wi-Fi mode to Station (STA)
                .ssid        = SYS_WINCS_WIFI_STA_SSID,        // Set the SSID (network name) for the Wi-Fi connection
                .passphrase  = SYS_WINCS_WIFI_STA_PWD,         // Set the passphrase (password) for the Wi-Fi connection
                .security    = SYS_WINCS_WIFI_STA_SECURITY,    // Set the security type (e.g., WPA2) for the Wi-Fi connection
                .autoConnect = SYS_WINCS_WIFI_STA_AUTOCONNECT  // Enable or disable auto-connect to the Wi-Fi network
            }; 

            // Set the Wi-Fi parameters
            if (SYS_WINCS_FAIL == SYS_WINCS_WIFI_SrvCtrl(SYS_WINCS_WIFI_SET_PARAMS, &wifi_sta_cfg))
            {
                g_appData.state = APP_STATE_WINCS_ERROR;
                break;
            }
            SYS_CONSOLE_PRINT("\r\n\r\n[APP] : Wi-Fi Connecting to : %s\r\n", SYS_WINCS_WIFI_STA_SSID);
            g_appData.state = APP_STATE_WINCS_SERVICE_TASKS;
            break;
        }

        case APP_STATE_WINCS_CREATE_SOCKET:
        {
            // Set the callback handler for NET socket events
            SYS_WINCS_NET_SockSrvCtrl(SYS_WINCS_NET_SOCK_SET_CALLBACK, SYS_WINCS_NET_SockCallbackHandler);

            // Create a TCP socket
            if (SYS_WINCS_FAIL == SYS_WINCS_NET_SockSrvCtrl(SYS_WINCS_NET_SOCK_TCP_OPEN, &g_tcpClientSocket))
            {
                g_appData.state = APP_STATE_WINCS_ERROR;
                break;
            }

            g_appData.state = APP_STATE_WINCS_SERVICE_TASKS;
            break;
        }

        case APP_STATE_WINCS_SERVICE_TASKS:
        {
            // Perform service tasks
            break;
        }
        
        case APP_STATE_WINCS_ERROR:
        {
            SYS_CONSOLE_PRINT(TERM_RED"[APP_ERROR] : ERROR in Application "TERM_RESET);
            g_appData.state = APP_STATE_WINCS_SERVICE_TASKS;
            break;
        }

        /* The default state should never be executed. */
        default:
        {
            /* TODO: Handle error in application's state machine. */
            break;
        }
    }
}


/*******************************************************************************
 End of File
 */