4.1.8.6.1 Wi-Fi System Interface
- SYS_WINCS_WIFI_MODE_t enum
- SYS_WINCS_WIFI_PARAM_t
- SYS_WINCS_WIFI_SECURITY_t struct
-
SYS_WINCS_WIFI_SCAN_PARAM_t structure
SYS_WINCS Wi-Fi Mode EnumSets the Wi-Fi mode of operationtypedefenum { SYS_WINCS_WIFI_MODE_STA, /**<Station (STA) mode of WiFi operation*/ SYS_WINCS_WIFI_MODE_AP, /**<Software Access Point (SoftAP) mode of WiFi operation*/ }SYS_WINCS_WIFI_MODE_t;WINCS Wi-Fi Parameters StructThe Wi-Fi parameters are listed below:typedef struct { /**< Wi-Fi operation mode ::SYS_WINCS_WIFI_MODE_t either STA (Station) or SoftAP (Software Access Point) */ SYS_WINCS_WIFI_MODE_t mode; /**< Wi-Fi SSID (Service Set Identifier) of Home AP (Access Point) or SoftAP */ const char *ssid; /**< Wi-Fi Passphrase of Home AP or SoftAP */ const char *passphrase; /**< Wi-Fi Security mode ::SYS_WINCS_WIFI_SECURITY_t */ SYS_WINCS_WIFI_SECURITY_t security; /**< Wi-Fi autoconnect flag, indicates whether to automatically connect to the network */ uint8_t autoConnect; /**< Wi-Fi channel number */ uint8_t channel; /**< SSID visibility flag, indicates whether the SSID is hidden (true) or visible (false) */ bool ssidVisibility; } SYS_WINCS_WIFI_PARAM_t;WINCS Wi-Fi Security EnumWi-Fi security modes.typedef enum { /**<OPEN mode, no security*/ SYS_WINCS_WIFI_SECURITY_OPEN = 0, /* WPA2 mixed mode (AP) / compatibility mode (STA) with PSK. * (As an AP GTK is TKIP, as a STA GTK is chosen by AP; * PTK can be CCMP or TKIP) */ SYS_WINCS_WIFI_SECURITY_WPA2_MIXED = 2, /* WPA2-only authentication with PSK. (PTK and GTK are both CCMP). */ /* Note that a WPA2-only STA will not connect to a WPA2 mixed mode AP. */ SYS_WINCS_WIFI_SECURITY_WPA2 = 3, /* WPA3 SAE transition mode. (CCMP, IGTK can be BIP or none) */ SYS_WINCS_WIFI_SECURITY_WPA3_TRANS = 4, /* WPA3 SAE authentication. (CCMP, IGTK is BIP) */ SYS_WINCS_WIFI_SECURITY_WPA3 = 5, } SYS_WINCS_WIFI_SECURITY_t;SYS_WINCS_WIFI_COEX_CFG struct Wi-Fi Bt coexistence confgurations.
SYS_WINCS_WIFI_COEX_CFG struct typedef struct { /** Indicates if 2-wire coexistence interface is used. */ bool use2Wire; /** Indicates if WLAN RX has higher priority than Bluetooth. */ bool wlanRxHigherThanBt; /** Indicates if WLAN TX has higher priority than Bluetooth. */ bool wlanTxHigherThanBt; /** Indicates if WLAN and Bluetooth share the same antenna. */ bool sharedAntenna; } SYS_WINCS_WIFI_COEX_CFG;SYS_WINCS_WIFI_SCAN_PARAM_t structure scan configurations.
SYS_WINCS_WIFI_SCAN_PARAM_t structure typedef struct { /**< Wi-Fi channel number to scan */ uint8_t channel; /**< Duration of the scan time in milliseconds */ uint16_t scanTime; } SYS_WINCS_WIFI_SCAN_PARAM_t;