6.1.1.1 Building and Running the TCP Client Application
To build this application, open the project file
(apps\tcp_client\firmware\tcp_client_sam_e54_xpro_wincs02.X/
) in
MPLAB X IDE. For more details on opening the project file in MPLAB X IDE, refer to the
Opening the
Project File. The following table provides details on the project file.
Project Name | Description |
---|---|
tcp_client_sam_e54_xpro_wincs02.X |
|
Running the Application
- Mount the WINCS02 Add On Board on SAM E54 Xplained Pro evaluation kit at respective header. For more details about the boards placement in the SAM E54 X-plained host board, see Figure
- Connect the debugger USB port on the SAM E54 Xplained Pro evaluation kit to computer using a micro-USB cable.
- Open the project and launch MCC Harmony3.
- Configure Home-AP credentials for STA mode, using the WINCS02 Wi-Fi configuration options. For more details about the Wi-Fi settings configuration, See Figure 4-25
- Configure TCP Server details such as TCP server IP address and port. For more details about the Net Sock settings configuration, See Figure 3-74.
- Generate the code as illustrated below.
Figure 6-2. Generating the Code - Build and program the code to the hardware using MPLABX IDE.
Figure 6-3. Programming the Board - Open the Terminal application (for example, Tera Term or PuTTY) on the PC
- Connect to the “EDBG Virtual COM Port” and configure the serial settings as
follows:
-
Baud: 115200
-
Data: 8 Bits
-
Parity: None
-
Stop: 1 Bit
-
Flow Control: None
-
- As the board boots up, it will
connect to Home-AP and print the IP address obtained. The board will establish a
connection with configured TCP Server and print a success message. Once the TCP
client-server connection is successful, the application will continue listening
on the socket for incoming messages and then write them back to the server.
Figure 6-4. TCP Client - Serial Logs