6.1.6.1 Building and Running the TLS Client Application
Building the Application
To build this application, open the project file
(
apps/tls_client/firmware/tls_client_sam_e54_xpro_wincs02.X/)
in MPLAB X IDE. For more details on opening the project file in MPLAB X IDE, refer
to the Opening
the Project File. The following table provides details on the project
file.| Project Name | Description |
|---|---|
tls_client_sam_e54_xpro_wincs02.X |
|
Running the Application
- Mount the WINCS02 Add On Board on SAM E54 Xplained Pro evaluation kit at respective header. For more details about the boards placement in the SAM E54 X-plained host board, see Figure 6-1.
- Connect the debugger USB port on the SAM E54 Xplained Pro evaluation kit to computer using a micro-USB cable.
- Open the project and launch MCC Harmony3.
- Configure Home-AP credentials for STA mode, using the WINCS02 Wi-Fi configuration options. For more details about the Wi-Fi settings configuration, See Figure 4-25.
- Generate the code as
illustrated below
Figure 6-29. Generating the Code 
- Build and program the code to
the hardware using MPLABX IDE
Figure 6-30. Programming the Board 
- Open the Terminal application
(for example, Tera Term or PuTTY) on the PC
Connect to the "EDBG Virtual COM Port" and configure the serial settings as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
- Press the Reset button on the host board, see Figure 6-1.
- As the board boots up, it
will connect to Home-AP and prints the IP address obtained. The board will
establish a connection with AWS S3. After establishing a successful TLS
server-client connection, the application will try to access/read the
document listed.
Figure 6-31. TLS Client Serial Logs - Once the device receives
entire document,
Receive Completemessage is printed on serial console as illustrated in the following figure.Figure 6-32. TLS Client Serial Logs