General Call
The general call is performed in order to change the address of the client.
If a GENERAL CALL is detected, GACC is set.
After the detection of general call, it is up to the user to decode the commands which follow.
In case of a WRITE command, the user has to decode the programming sequence and program a new SADR if the programming sequence matches.
The following figure describes the general call access.
Note: This method enables to create a
user-specific programming sequence by choosing the number of programming bytes. The
programming sequence has to be provided to the host.