1.2 Drive Transistor Failure
An external transistor is used to switch the relay position. If the transistor fails
short, these failures could be detected by matching the internal output value of the I/O
pin (LATx) with the actual value of the I/O pin (PORTx). For instance, if the internal
output value of LATx is ‘1’, but the transistor is shorted to ground,
then the output state seen by the digital logic (PORTx) is ‘0’.
CAUTION: If the relay coil is driven by a higher voltage
than the microcontroller, a short between the drain and gate could expose the
microcontroller to a voltage that exceeds its absolute maximum rating. If this failure
mode is anticipated, current-limiting resistors, Zener diodes and/or other protection
devices can protect the I/O pins.