7.1 List of Unmounted Elements

Two types of unmounted components are listed in this section:

  • In blue, the components that can be mounted, with some board adaptation, without any damage to the system.
  • In red, unmounted components used for factory and debug configuration. Those should never be mounted, as such action could result in damage or destruction of the board or system elements.
Figure 7-1. Unmounted Components Overview: Top View

The following table lists the top side unmounted components and their functionalities.

Table 7-1. Top Side Unmounted Elements
Ref.TypeFeatureColor StatusUsed forWhat to do if mounted
C76Capacitor24 MHzBlueCrystal load capacitanceRemove R34 and R36.
C81Capacitor24 MHzBlueCrystal load capacitance
R37Resistor24 MHzBlueCrystal selection
R40Resistor24 MHzBlueCrystal selection
Y3Crystal24 MHzBlue24 MHz crystal
R39Resistor24 MHzRedCrystal measurementOnly use in factory. If mounted, the crystal behavior will be degraded.
C165Capacitor25 MHz RGMIIBlueCrystal load capacitanceRemove R171.
C166Capacitor25 MHz RGMIIBlueCrystal load capacitance
R167Resistor25 MHz RGMIIBlueCrystal selection
R168Resistor25 MHz RGMIIBlueCrystal selection
Y5Crystal25 MHz RGMIIBlue25 MHz crystal
C192Capacitor25 MHz RMIIBlueCrystal load capacitanceRemove R178.
C193Capacitor25 MHz RMIIBlueCrystal load capacitance
R181Resistor25 MHz RMIIBlueCrystal selection
R184Resistor25 MHz RMIIBlueCrystal selection
Y8Crystal25 MHz RMIIBlue25 MHz crystal
R183Resistor25 MHz RMIIRedCrystal measurementOnly use in factory. If mounted, the crystal behavior will be degraded.
R35Resistor32 kHzRedCrystal measurementOnly use in factory. If mounted, the crystal behavior will be degraded.
U20ModuleATWILC3000BlueATWILC3000 module–
J15ConnectorDebugBlueWILC3000 debug interface–
J16ConnectorDebugBlueWILC3000 debug interface–
R232ResistorDebugBlueDebug CTS pull-up–
R233ResistorDebugBlueDebug RTS pull-up–
R179ResistornRST_OUTBluenRST selection instead of NRST_OUTRemove R180.
R118ResistorSD CardRedSDMMC1_1V8_SEL pull-up–
C127CapacitorSupplyRedVLDO1 decoupling

–

Note: Excessive capacitor load on the MCP16502 DCDC or LDO lines can result in output instability and power-on sequence failure.

C128CapacitorSupplyRedVDD_3V3 decoupling
C220CapacitorSupplyRedVDD_3V3_WILC decoupling
C240CapacitorSystemBluenSTART decoupling and startup configurationThe product starts automatically.
J14ConnectorTamperBlueTamper pins use–
R164ResistorEthernet RGMIIRedGigabit Ethernet 125 MHz clock line–
Figure 7-2. Unmounted Components Overview: Bottom View

The following table lists the bottom side unmounted components and their functionalities.

Table 7-2. Bottom Side Unmounted Elements
Ref.TypeFeatureColor StatusUsed forWhat to do if mounted
C77Capacitor32 kHzBlueMEMS oscillator decouplingRemove Y1, C66 and C72.
R38Resistor32 kHzBlueMEMS oscillator selection
Y4MEMS oscillator32 kHzBlue32 kHz MEMS generation
R266ResistorDebugRedJTAG TCK pull-up
R249ResistorJ-Link-OBRedBoundary scan selectionIf mounted, at boot the device enters in boundary scan. J-Link-OB will never start.
R134ResistornRST_OUTBluenRST selection instead of NRST_OUTRemove R136.
R165ResistornRST_OUTBluenRST selection instead of NRST_OUTRemove R166.
R198ResistornRST_OUTBluenRST selection instead of NRST_OUTRemove R199.
R119ResistornRST_OUTBlueNRST_OUT selection instead of SDMMC1_RSTN_PB28If mounted, the SD Card can also be reset by the processor reset line.
R24ResistornRST_OUTRednRST_OUT pull-upNo impact
R10ResistorPMICRedPMIC output voltage selectionNever mount this element. The VLDO1 output voltage is set to 1.8V for SD Card voltage selection. If changed, the SD Card interface might get destroyed.
C103CapacitorSAMA7G5BlueDDR_VERF decouplingNo impact
C123CapacitorSAMA7G5RedDDR_VERF decoupling
C124CapacitorSAMA7G5RedDDR_VERF decoupling
R26ResistorSAMA7G5RedBoundary scan selectionIf mounted, at boot the device enters in boundary scan.
R191ResistorSupplyBlueInput supply selectionRemove R185.
C167CapacitorSupplyRedAVDDH decoupling

–

Note: Excessive capacitor load on the MCP16502 DCDC or LDO lines can result in output instability and power-on sequence failure.

C177CapacitorSupplyRedDVDDH decoupling
R148ResistorEthernet RGMIIRedTXCK pull-up–
R153ResistorEthernet RGMIIBlueRXCTL pull-up–