4.2 Board Setup
Follow these steps before using the SAMA7G54-EK:
- Unpack the board, taking care to avoid electrostatic discharge.
- Check the Default Jumper Settings.
- Connect the USB-micro-AB cable to connector J24 (J-Link-OB USB port).
- Connect the other end of the cable to a free port on the PC.
- Open a terminal (console 115200, N, 8, 1) on the PC.
- Supply the board by performing one of
the following connections:
- USB-micro-AB cable to connector J7 (USB-A port)
- AC/DC wall adapter to connector J1 (DC jack connector)
- Reset the board.
- A startup message appears on the console as shown in the picture below.