6.1.1.5 Movff/movffl Instructions
The movff
instruction is a physical device instruction,
but for PIC18 devices that have extended data memory, it also serves as a placeholder for
the movffl
instruction.
For these devices, when generating output for the movff
instruction, the assembler checks the psects that hold the operand symbols. If the psect
containing the source operand and the psect containing the destination operand both specify
the lowdata
psect flag, the instruction is encoded as the two-word
movff
instruction. If an operand is an absolute address and that
address is in the lower 4 KB of memory, then that is also considered acceptable for the
shorter form of the instruction. In all other situations, the instruction is encoded as a
three-word movffl
instruction.
Note that assembly list files will always show the movff
mnemonic, regardless of how it is encoded. Check the number of op-code words to determine
which instruction was encoded.