6.3.6.3 Call Graph Graphs

Following the call tables are the call graphs, which show the full call tree for main() and any interrupt functions. This is a subset of the information presented in the call tables, and it is shown in a different form. The call graphs will look similar to the one shown below.

CALL GRAPH GRAPHS

Indentation is used to indicate the call depth. In the diagram, you can see that main() calls aOut(), which in turn calls GetDACValue(), which in turn calls the library function __ftadd(), etc. If a star (*) appears next to the function’s name, this implies that the function has been called indirectly via a pointer.