9.2.13 __debug_break Builtin
A builtin function that triggers a software breakpoint for debug builds.
Include
<xc.h>
Prototype
void __debug_break(void);
Remarks
This is an inbuilt function that is expanded by the code generator for debug builds, but is ignore for production builds. When called, this routine unconditionally triggers a software breakpoint when the code is executed using a debugger.
The software breakpoint code is only generated for mid-range and PIC18 devices. Baseline devices do not support software breakpoints in this way, and the builtin will be ignored if used with these devices.
Example
The following example shows different types of breakpoints added to an
MCC-generated function.
#include <xc.h>
static i2c1_fsm_states_t I2C1_DO_BUS_COLLISION(void)
{
// Clear bus collision status flag
I2C1_MasterClearIrq();
I2C1_Status.error = I2C1_FAIL;
switch (I2C1_Status.callbackTable[I2C1_WRITE_COLLISION](I2C1_Status.callbackPayload[I2C1_WRITE_COLLISION])) {
case I2C1_RESTART_READ:
return I2C1_DO_SEND_RESTART_READ();
case I2C1_RESTART_WRITE:
__debug_break(); /* break when debugging only */
return I2C1_DO_SEND_RESTART_WRITE();
default:
__builtin_software_breakpoint(); /* unconditional break */
return I2C1_DO_RESET();
}
}