5.14.3.4 The #pragma Intrinsic Directive
The #pragma intrinsic directive is used to indicate to
the compiler that a function will be inlined intrinsically by the compiler. This directive
should never be used with user-defined code.
You should not attempt to redefine an existing library function that uses
the intrinsic pragma. If you need to develop your own version of such a
routine, it must not use the same name as the intrinsic function. For example, if you need
to develop your own version of memcpy(), give this a unique name, such as
sp_memcpy(). Check the standard header files to determine which library
functions use this pragma.