5.14.3.8 The #pragma Psect Directive
The #pragma psect was used to redirect objects and
functions to a new psect (section). It has been replaced by the
__section() specifier (see Changing and Linking the Allocated Section), which not only performs the same
task, but is easier to use, and has fewer restrictions as to where the psects can be
linked. It is recommended you always use the __section() specifier to
location variables and function in unique psects.
The general form of this pragma looks like:
#pragma psect standardPsect=newPsect
and instructs the code generator that anything that would normally appear
in the standard psect standardPsect, will now appear in a new psect called
newPsect. This psect will be identical to
standardPsect in terms of its flags and attributes; however, it will
have a unique name. Thus, you can explicitly position this new psect without affecting the
placement of anything in the original psect.
If the name of the standard psect that is being redirected contains a
counter (e.g., text0, text1, text2,
etc.), the placeholder %%u should be used in the name of the psect at the
position of the counter, e.g., text%%u.