4.6.1.2 Checksum Option
-mchecksum=specs option calculates a
hash value (for example checksum or CRC) over the address range specified and stores the
result in the hex file at the indicated destination address. The general form of this
option is as
follows.-mchecksum=start-end@destination[,specifications]The start, end and
destination attributes are, by default, hexadecimal
constants. The addresses defining the input range (start -
end) are typically made multiples of the algorithm width. If this is
not the case, bytes (with value 0) will pad any missing input word locations. The
destination is where the hash result will be stored. This address
cannot be within the range of addresses over which the hash is calculated.
The following specifications are appended as a comma-separated list to this option.
| Argument | Description |
|---|---|
width=n | Optionally specifies a decimal width of the result. The width can be specified as 1 to 8 bytes for most algorithms, but it represents the bit width for SHA algorithms. If a positive width is requested, the result will be stored in big-endian byte order. A negative width will cause the result to be stored in little-endian byte order. If the width is left unspecified, the result will be 2 bytes wide and stored in little-endian byte order. This width argument is not required with any Fletcher algorithm, as they have fixed widths, but it may be used to alter the default endianism of the result. |
offset=nnnn | Specifies an initial hexadecimal value or offset to be used in the hash calculation. It is not used with SHA algorithms. |
algorithm=n | The decimal argument selects one of the hash algorithms implemented in Hexmate. The selectable algorithms are described in the following table. If unspecified, the default algorithm used is 8-bit checksum addition (algorithm 1). |
polynomial=nn | Selects the polynomial value when using CRC algorithms |
code=nn.Base | Selects a hexadecimal code that will trail
each byte in the result. This can allow each byte of the hash result to be
embedded within an instruction, for example code=34 will embed
each byte of the result in a retlw instruction on Mid-range
devices, or code=0000 will append two 0x00 bytes to each byte
of the hash. This code sequence can be optionally followed by
.Base, where Base is the
number of bytes of the hash to be output before the trailing code sequence is
appended. A specification of code=1122.2, for example, will
output the bytes 0x11 and 0x22 after each two bytes of the hash result. |
revword=n | Specifies a decimal word width. If this is non-zero, then
bytes within each word are read in reverse order when calculating a hash value.
Words are aligned to the addresses in the HEX file. The width must be either 0
or an integer greater than 1. Typical values would be 2 or 4, depending on the
application. It is recommended that you do not exceed a width of 8. A zero
width disables the reverse-byte feature, as if the revword
suboption was not present. This suboption should be used when using Hexmate to
match a CRC produced by a PIC hardware CRC module that use the Scanner module
to stream data to it. |
skip=n.Bytes | Specifies a decimal word width. If this is non-zero, then the
MSB within each word is skipped for the purposes of calculating a hash value.
Words are aligned to the addresses in the HEX file. At present, the width must
be 0 (which disables the skip feature, as if the skip
suboption was not present) or greater than 1. This value can be optionally
followed by .Bytes, where
Bytes is a number representing the
number of bytes to skip in each word; for example, skip=4.2
will skip the two most significant bytes in each 4-byte word. |
xor=n | Specifies a hexadecimal value (a leading 0x
or 0X prefix is optional) that will be XORed with CRC results
before it is stored. XORs cannot be performed when using other
algorithms. |
Note that the words acted on by the reverse and skip features are aligned to HEX file
addresses, not to their position in the sequence being processed. In other words, what
constitutes a data word is not affected by the start and
end addresses specified with the option.
If an accompanying --fill option (Fill Option) has not been specified, unused
locations within the specified address range will be automatically filled with 0xFFF for
baseline devices, 0x3FFF for mid-range devices, or 0xFFFF for PIC18 devices. This is to
remove any unknown values from the calculations and ensure the accuracy of the result.
For example:
-mchecksum=800-fff@20,width=1,algorithm=2will calculate a 1-byte checksum from address 0x800 to 0xfff and store this at address 0x20. A 16-bit addition algorithm will be used. The table below shows the available algorithms and Hash Value Calculations describes these in detail.
| Selector | Algorithm description |
|---|---|
-5 | Reflected cyclic redundancy check (CRC) |
-4 | Subtraction of 32 bit values from initial value |
-3 | Subtraction of 24 bit values from initial value |
-2 | Subtraction of 16 bit values from initial value |
-1 | Subtraction of 8 bit values from initial value |
1 | Addition of 8 bit values from initial value |
2 | Addition of 16 bit values from initial value |
3 | Addition of 24 bit values from initial value |
4 | Addition of 32 bit values from initial value |
5 | Cyclic redundancy check (CRC) |
7 | Fletcher’s checksum (8 bit calculation, 2-byte result width) |
8 | Fletcher’s checksum (16 bit calculation, 4-byte result width) |
10 | SHA-2 (currently only SHA256 is supported) |
11 | SHA-1 (160 bit) |
The hash calculations described above are performed by the Hexmate utility. Further information regarding how hashes are calculated can be found in Ck Hexmate Option.