3.3.5.2 How Do I Stop An Unused Function Being Removed?
If a C function’s symbol is referenced in hand-written assembly code, the function will never be removed, even if it is not called or has never had its address taken in C code.
To include a reference, create an assembly source file and add this file to your project. You only have to reference the symbol in this file; so the file can contain the following
GLOBAL _myFunc
where myFunc is the C name of the function in question
(note the leading underscore in the assembly name, see Equivalent Assembly Symbols). This is sufficient to
prevent the function removal optimization from being performed.