6.1.9.17 Error Directive
The error directive produces a user-defined build-time error message
that will halt the assembler. The message to be printed should this directive be
executed is specified as a string. Typically this directive will be made conditional, to
detect an invalid situation.
For
example:
IF MODE
call process
ELSE
ERROR "no mode defined"
ENDIF