7.3.2.3 Psect Information Listed By Class
The next section in the map file shows the same psect information but grouped by the psects’ class.
This section is heralded by the line that contains the headings:
TOTAL Name Link Load Length
Under this are the class names followed by those psects which belong to this class (see Class Flag). These psects are the same as those listed by module in the above section; there is no new information contained in this section, just a different presentation.