4.6.1.11 Heap Option
The -mheap=[size|auto] option specifies
the size of memory reserved for the heap.
The heap is used with the standard dynamic memory allocation functions,
those being malloc(), calloc(),
realloc(), and free(), whose operation is described in
Dynamic Memory Allocation for PIC Devices.
When this option is used with a size argument, being a
decimal number of bytes, the compiler will attempt to reserve the requested amount of
memory for the heap. Thus, at runtime, the heap will be able to grow to the specified size
with no corruption of data. This memory is reserved unconditionally, even if no dynamic
memory allocation functions are used in the program.
Alternatively, the argument may be specified as auto, in which case the
compiler will calculate a maximum size for the heap after other static and stack
allocations have been made. Memory with this calculated size will only be reserved,
however, if the compiler detects calls to any of the dynamic memory allocation functions in
the program. If no -mheap option is specified, then the compiler uses an
auto setting, as if -mheap=auto was issued. Whenever acting with an auto
setting, the compiler will issue a compiler advisory message if dynamic memory allocation
functions have been detected and memory has been reserved as a result.
The size of software stacks used by functions compiled to use a reentrant model are also
dynamic in nature, and memory must be reserved for their use. That memory is specified
using the -mstack option (see Stack Option). A size argument of
auto can be used with both the -mheap and
-mstack options, in which case the compiler will evenly distribute the
free memory remaining between the heap and stacks after other statical allocations have
been made.