4.6.1.6 Debugger Option
The -mdebugger=type option is intended
for use in compatibility with development tools that can act as a debugger.
xc8-cc supports several debuggers and these are defined in the table
below. Failing to select the appropriate debugger can lead to runtime failure.
| Type | Debugger selected |
|---|---|
none | No debugger (default) |
icd2 | MPLAB® ICD 2 |
icd3 | MPLAB ICD 3 |
icd4 | MPLAB ICD 4 |
icd5 | MPLAB ICD 5 |
pickit2 | PICkit™ 2 |
pickit3 | PICkit 3 |
pickit4 | PICkit 4 |
pickit5 | PICkit 5 |
realice | MPLAB REAL ICE™ In-circuit Emulator |
ice4 | MPLAB ICE 4 In-circuit Emulator |
snap | MPLAB Snap |
xc8-cc -mcpu=16F1946
-mdfp="Microchip/PIC12-16F1xxx_DFP/1.7.242/xc8" -mdebugger=icd5 main.cwill
ensure that none of the source code is allocated resourced that would be used by the debug
executive for an MPLAB ICD 5.When a debugger is set using this option, a preprocessor macro is defined, allowing your source code to change based on the debugger selection, see Predefined Macros.
If the debugging features of the development tool are not to be used (for
example, if the MPLAB ICD 5 is only being used as a programmer), then the debugger option
can be set to none, because memory resources will not be used by the tool
in that situation.