6.1.9.49 Warn Directive
The WARN directive produces a user-defined build-time warning message.
Execution of this directive will not prevent the compiler
from building. The warning to be printed should this directive be executed is specified
as a string. Typically this directive will be made conditional, to detect an invalid
situation.
For example:
IF MODE
movwf modeQ
ELSE
WARN "MODE is zero - write skipped"
ENDIF