8.2.3.9 Werror Option
The --werror option can be used to promote compiler
warnings into errors. As with any other error, these promoted messages will prevent the
application from completing.
The --werror form of this option promotes all compiler warning messages issued into errors. This option might be useful in
applications where warnings are not permitted for functional safety reasons.
The --werror=num form of this option promotes only the
warning identified by num to an error. See a list of
messages and their corresponding number in the Error and Warning Messages
section towards the end of this document. If the message indicated by
num is not a warning, then this option has no
effect. Only one message number may be specified with this option; however, you may use
this option as many times as required.
The --wno-error=num form of this option ensures that
the warning identified by num is never promoted to an
error, even if the --werror form of this option is in effect.