5.1.2.3 Const Auto Objects
If a Baseline or Mid-range device is selected, any auto
objects that are specified as const are treated
as if they were also specified static. This
does not affect the scope of the object, but does imply that its
value will be stored in program memory and any initializer
assigned to the variable when it is defined must be a constant
expression.
This limitation does not affect projects using PIC18 devices, since
const auto objects with these
devices are stored in data memory.