6.3.4 Switch Statement Information
Along with the generated code for each switch statement
is information about how that statement was encoded. There are several strategies the
compiler can use for switch statements. The compiler determines the
appropriate strategy (see Switch Statements) or you can indicate a preference for a particular type of
strategy using a pragma (see The #pragma Switch Directive). The information printed will look similar to the figure
shown below.