6.1.9.29 Macro And Endm Directives
The MACRO … ENDM directives provide for the definition of
assembly macros, optionally with arguments. See Equ Directive for simple association of
a value with an identifier, or Preprocessor Directives
for the preprocessor’s #define macro directive, which can also
work with arguments.
The MACRO directive should be preceded by the macro name
and optionally followed by a comma-separated list of formal arguments. When the
macro is used, the macro name should be used in the same manner as a machine
opcode, followed by a list of arguments to be substituted for the formal
parameters.
;macro: movlf - Move a literal value into a nominated file register
;args: arg1 - the literal value to load
; arg2 - the NAME of the source variable
movlf MACRO arg1,arg2
movlw arg1
movwf arg2 mod 080h
ENDMmovlf 2,tempvarexpands
to:movlw 2
movwf tempvar mod 080h& character can be used to permit the
concatenation of macro arguments with other text, but is removed in the actual
expansion. For example:loadPort MACRO port, value
movlw value
movwf PORT&port
ENDMwill load PORTA if port is
A when called, etc. The special meaning of the
& token in macros implies that you can not use the
bitwise AND operator, (also represented by
&), in assembly macros; use the and form of
this operator instead.A comment can be suppressed within the expansion of a macro (thus saving
space in the macro storage) by opening the comment with a double semicolon,
;;.
When invoking a macro, the argument list must be comma-separated. If it is
desired to include a comma (or other delimiter such as a space) in an argument
then angle brackets < and > can be used to
quote
See Local Directive for use of unique local labels within macros.
By default, the assembly list file will show macro in an unexpanded
format; i.e., as the macro was invoked. Expansion of the macro in the listing file
can be shown by using the EXPAND assembler directive (see Expand Directive).