3.5.21 How Do I Know What Value Has Been Programmed in the Configuration Bits or ID Location?

Check the assembly list file for the output of the #pragma config directives. You will see the numerical value programmed to the appropriate locations. In the following example, the configuration value programmed is 0x1F. A breakdown of what this value means is also printed in this file.

;Config register CONFIG2H @ 0x300003
;      Watchdog Timer Enable bit
; ...
;      WDTPS = 0xF, unprogrammed default
psect   config
org 3145731
db  31