7.4.9 EEPROM Objects
The __eeprom
qualifier can be used to indicate that variables should be
positioned in EEPROM.
Use the native keywords discussed in the Differences section to look up information on the semantics of this qualifier.
Some devices may not implement EEPROM. Use of this qualifier for such devices generates a
warning. Stack-based (auto
and parameter) variables cannot use the
__eeprom
specifier.
Example
The following shows a variable qualified using __eeprom
.
__eeprom int serialNos[4];
Differences
When targeting PIC devices, the MPLAB XC8 compiler has used the eeprom
qualifier to indicate that objects should be placed in EEPROM.
The MPLAB XC16 and XC-DSC compilers have used the space
attribute to
allocate variables to the memory space used for EEPROM.
Migration to the CCI
When using MPLAB XC8 to build for PIC devices, change any occurrence of the
eeprom
qualifier to __eeprom
, for example,
from:
eeprom char title[20];
to:
__eeprom char title[20];
When using MPLAB XC16 or XC-DSC compilers, change any occurrence of the eedata
space
attribute to the __eeprom
specifier, for example,
from:
int mainSw __attribute__ ((space(eedata)));
to:
int __eeprom mainSw;
Caveats
The MPLAB XC8 compiler only permits the __eeprom
specifier for those
Baseline and Mid-range devices that support this memory. It is not permitted for other
8-bit devices.