8.1.1 Example code for 8-bit AVR MCUs
The UART IO feature in the MPLAB X IDE allows you to view output from the
stdout
stream. Once properly configured, the output of
printf()
and other functions can then be viewed from the IDE when
the program is run in the simulator.
This feature is enabled from Project properties > Simulator > USARTx IO Options. You might have a choice of USARTs. Choose the USART that your code will write to. Output can be displayed in a window in the IDE or sent to a file on your host machine, based on the selections you make in the dialog.

The USART initialization and print-byte function generated by the MCC will allow
printf()
to work in the simulator. If you enable the
Printf support checkbox in the USART dialog, MCC will
generate the necessary mapping via the FDEV_SETUP_STREAM()
macro to
ensure that printf()
calls the correct print-byte function. The default
communication settings should work in the simulator, but these may need to be changed if
the USART is to be used on hardware.