“The number of bits in a byte (C90 3.4, C99
3.6).” |
| 8. |
“The values of the members of the execution
character set (C90 and C99 5.2.1).” |
| The execution character set is ASCII. |
“The unique value of the member of the execution
character set produced for each of the standard alphabetic escape sequences
(C90 and C99 5.2.2).” |
| The execution character set is ASCII. |
“The value of a char object into
which has been stored any character other than a member of the basic execution
character set (C90 6.1.2.5, C99 6.2.5).” |
| The value of the char object is the 8-bit binary
representation of the character in the source character set. That is, no
translation is done. |
“Which of signed char or
unsigned char has the same range, representation, and behavior as
“plain” char (C90 6.1.2.5, C90 6.2.1.1, C99 6.2.5, C99
6.3.1.1).” |
| By default, signed char is functionally equivalent to
plain char . If the CCI is specified, then the default is
unsigned char The options -funsigned-char
and -fsigned-char can be used to explicitly specify the
type. |
“The mapping of members of the source character
set (in character constants and string literals) to members of the execution
character set (C90 6.1.3.4, C99 6.4.4.4, C90 and C99 5.1.1.2).” |
| The binary representation of the source character set is preserved to the
execution character set. |
“The value of an integer character constant
containing more than one character or containing a character or escape sequence
that does not map to a single-byte execution character (C90 6.1.3.4, C99
6.4.4.4).” |
| The previous value is shifted left by eight, and the bit pattern of the
next character is masked in. The final result is of type int .
If the result is larger than can be represented by an int , a
warning diagnostic is issued and the value truncated to int
size. |
“The value of a wide character constant containing
more than one multibyte character, or containing a multibyte character or
escape sequence not represented in the extended execution character set (C90
6.1.3.4, C99 6.4.4.4).” |
| Multi-byte characters are not supported in source files. |
“The current locale used to convert a wide
character constant consisting of a single multibyte character that maps to a
member of the extended execution character set into a corresponding wide
character code (C90 6.1.3.4, C99 6.4.4.4).” |
| Multi-byte characters are not supported in source files. |
“The current locale used to convert a wide string
literal into corresponding wide character codes (C90 6.1.4, C99
6.4.5).” |
| Wide strings are not supported. |
“The value of a string literal containing a
multibyte character or escape sequence not represented in the execution
character set (C90 6.1.4, C99 6.4.5).” |
| Multi-byte characters are not supported in source files. |