1.1 Conventions Used in This Guide
The following conventions may appear in this documentation. In most cases, formatting conforms to the OASIS Darwin Information Typing Architecture (DITA) Version 1.3 Part 3: All-Inclusive Edition, 19 June 2018.
Description | Implementation | Examples |
---|---|---|
References | DITA: cite | MPLAB® XC8 C Compiler User’s Guide for AVR® MCU. |
Emphasized text | Italics | ...is the only compiler... |
A window, window pane or dialog name. | DITA: wintitle | the
Output window. the New Watch dialog. |
A field name in a window or dialog. | DITA: uicontrol | Select the Optimizations option category. |
A menu name or item. | DITA: uicontrol | Select the File menu and then Save. |
A menu path. | DITA: menucascade, uicontrol | |
A tab | DITA: uicontrol | Click the Power tab. |
A software button. | DITA: uicontrol | Click the OK button. |
A key on the keyboard. | DITA: uicontrol | Press the F1 key. |
File names and paths. | DITA: filepath | C:/Users/User1/Projects |
Source code: inline. | DITA: codeph | Remember to
#define START at the beginning of your
code. |
Source code: block. | DITA: codeblock | An example
is:
|
User-entered data. | DITA: userinput | Type in a device name, for example PIC18F47Q10. |
Keywords | DITA: codeph | static , auto ,
extern |
Command-line options. | DITA: codeph | -Opa+, -Opa- |
Bit values | DITA: codeph | 0,
1 |
Constants | DITA: codeph | 0xFF,
'A' |
A variable argument. | DITA: codeph + option | file.o , where
file can be any valid file
name. |
Optional arguments | Square brackets [ ] | xc8
[options]
files |
Choice of mutually exclusive arguments; an OR selection. | Curly brackets and pipe character: { | } | errorlevel {0|1} |
Replaces repeated text. | Ellipses... | var_name [,
var_name...] |
Represents code supplied by user. | Ellipses... | void
main (void)
|
A number in verilog format, where N is the total number of digits, R is the radix and n is a digit. | N‘Rnnnn | 4‘b0010, 2‘hF1 |
Device Dependent insignia. Specifies that a feature is not supported on all devices. Please see your device data sheet for details. | [DD] | Assembler Special Operators |