4.3.3 Boolean Types

The compiler supports _Bool, a type used for holding true and false values.

The values held by variables of this type are not integers and behave differently in expressions compared to similar expressions involving integer types. Integer values converted to a _Bool type result in 0 (false) if the integer value is 0; otherwise, they result in 1 (true).

The <stdbool.h> header defines true and false macros that can be used with _Bool types and the bool macro, which expands to the _Bool type. For example:
#include <stdbool.h>
_Bool motorOn;
motorOn = false;