3.4.1 Output Files
The common output file types and case-sensitive extensions are shown in Table 3-2.
| Extension | File Type | How created |
|---|---|---|
.hex | Intel HEX | avr-objcopy application |
.elf | ELF (Executable and Linkable Format) with Dwarf debugging information | -o option |
.s | Assembly file | -S option |
.i | Preprocessed C file | -E and -o option |
The default behavior of is to produce an ELF file called
a.out, unless you override that name using the xc8-cc-o
option.
The ELF/DWARF file is used by debuggers to obtain debugging information about the project and allows for more accurate debugging compared to other formats, such as COFF. Some aspects of the project’s operation might not even be available to your debugger when using COFF. Development environments will typically request the compiler to produce an ELF file.
The names of many output files use the same base name as the source file
from which they were derived. For example the source file input.c will
create a file called input.o
when the -c option is used.