8.4.1 _delay_ms Function
Delay for the specified time.
Include
<util/delay.h>
Prototype
void _delay_ms(double ms);
ms- The time in milli seconds to delay.
Remarks
This function delays execution by using the _delay_loop_2()
function. The macro F_CPU should be defined as a constant that
specifies the CPU clock frequency (in Hertz). The compiler optimizers must be enabled
for accurate delay times.
The maximal possible delay is 4294967.295 ms/F_CPU in MHz. Requesting
values greater than the maximal possible delay will result in overflow and a delay of
0us.
Conversion of the requested number of milli seconds into clock cycles may not always result in integer value. By default, the number of clock cycles is rounded up to next integer. This ensures that there is at least the requested amount of delay.
By defining the macro __DELAY_ROUND_DOWN__, or
__DELAY_ROUND_CLOSEST__, before including this header file, the
algorithm can be made to round down, or round to closest integer, respectively.
Example
#define F_CPU 4000000UL
#include <util/delay.h>
int main(void)
{
_delay_ms(20); // delay for 20 milli seconds
}