8.7.1 set_sleep_mode Macro
Specify how the device is to behave in sleep mode.
Include
<avr/sleep.h>
Prototype
void set_sleep_mode(mode);
Remarks
This macro sets the appropriate bits in the device registers to specify how
the device will behavein sleep mode. The mode argument can be the appropriate macros
defined once you include <avr/sleep.h>, such as
SLEEP_MODE_IDLE, SLEEP_MODE_PWR_DOWN,
SLEEP_MODE_PWR_SAVE, SLEEP_MODE_STANDBY, etc.
Example
#include <xc.h>
#include <avr/sleep.h>
int main(void)
{
set_sleep_mode(SLEEP_MODE_IDLE);
cli();
if (some_condition)
{
sleep_enable();
sei();
sleep_cpu();
sleep_disable();
}
sei();
}