4.2.5 Configuration Bit Access

Configuration bits or fuses are used to set up fundamental device operation, such as the oscillator mode, watchdog timer, programming mode, and lockbit code protection. These bits must be correctly set to ensure your program executes correctly.

Use the configuration pragma, which has the following form, to set up your device.

#pragma config setting = state|value

Here, setting is a configuration setting descriptor, e.g., WDT, and state is a textual description of the desired state, e.g., SET. Those states other than SET and CLEAR are prefixed with the setting descriptor, as in BODLEVEL_4V3, as shown in the following examples.

#pragma config WDTON = SET
#pragma config EESAVE = CLEAR
#pragma config BODLEVEL = BODLEVEL_4V3
#pragma config LB = LB_NO_LOCK

The settings and states associated with each device can be determined from an HTML guide. Open the device-specific HTML file located in the xc8/avr/chipinfo directory of your selected DFP. This page will show you the settings and values that are appropriate with this pragma. Review your device data sheet for more information.

One pragma can be used to program several settings by separating each setting-value pair with a comma. For example, the above could be specified with one pragma, as in the following.

#pragma config WDTON=SET, EESAVE=CLEAR, BODLEVEL=BODLEVEL_4V3, LB=LB_NO_LOCK

The value field is a constant that can be used in preference to a descriptor, as in the following.

#pragma config SUT_CKSEL = 0x10

Setting-value pairs are not scanned by the preprocessor and they are not subject to macro substitution. The setting-value pairs must not be placed in quotes.

The config pragma does not produce executable code, and ideally it should be placed outside function definitions.

Those bits not specified by a pragma are assigned a default value. Rather than rely on this default value, all the bits in the Configuration Words should be programmed to prevent erratic program behavior.