1 Known Issues for MCC Melody 8-Bit MDFU Client Library
Provides a list of known issues in the 8-Bit MDFU Client Library.
- Issue:
M8BTL-4245
Issue Title:
Flash_Read in verification can cause corruption of the application interrupt logic on the AVR devices with memory that exceeds 0x10000 bytes.
Issue Description:
There is an existing issue for AVR devices that have larger flash memories where the RAMPZ register is set during verification sequences and it is never cleared. This causes interrupts to not be serviced correctly by the ISRs of the application code.
Workaround:
Clear the RAMPZ register inside of the FLASH_Read function found inside of the mcc_generated_files/nvm/src/nvm.c file.flash_data_t FLASH_Read(flash_address_t address) { // Workaround: // Store the read result flash_data_t result = pgm_read_byte_far(address); // Clear RAMPZ RAMPZ = 0; // Return the data byte return result; }
- Issue:
M8BTL-4075
Issue Title:
DFU failure for K22 devices due to incorrect initialization of IOC functionality on Port B
Issue Description:
In the PIC18FxxK22 series of devices, the PIN_MANAGER_Initialize() initializes the Port B Interrupt-On-Change (IOCx) Interrupt Enable bit (RBIE). This causes an interrupt to occur but its not serviced anywhere in the firmware causing the device to re-enter the same ISR on repeat. This prevents further execution of the non ISR code.
Workaround:
Comment out the line that sets the RBIE bit in the PIN_MANAGER_Initialize() function.
- Issue:
M8BTL-4076
Issue Title:
MDFU I2C com_adapter experiences failures when the delay timing is set to a very large number
Issue Description:
The MDFU Client firmware can experience an issue if the inter-message delay value of the FTP is set to a value that is too large. This issue creates a failure message on the host but the update is still successful.
Workaround:
None.
- Issue:
M8BTL-4067
Issue Title:
A few K-Series devices do not generate correct I2C register configurations causing the DFU operation to fail.
Issue Description:
There is a set of K series devices including the K22 and K80, that will generate their driver code with incorrect register initializations. There is no active workaround yet, but plans have been made to fix these issues at the driver level, so there are no plans to change the MDFU driver code as of now.
Workaround:
There is no active workaround to this issue as the register initializations could vary from implementation to implementation. Please look into your specific device data sheet for your required I2C register configurations.
- Issue:
M8BTL-3945
Issue Title:
The Read API in the PIC18F NVM driver can cause crashes during the verification due to the TBLPTR when interrupts are being used.
Issue Description:
The Flash_Read() function in the nvm.c file can create device crashes when the global interrupts are enabled. This causes an error where the bootloader can successfully load a new application, but it is unable to communicate that verification status back to the host. The bootloader is still able to verify the application and run the end application, but sending that status back to the host is not possible.
Workaround:
The workaround to resolve this issue us to simply disable the global interrupts while the TBLPTR is being used in the function:
static void CRC32_Calculate(flash_address_t startAddress, uint32_t length, uint32_t *crcSeed) { uint32_t byteIndex; for (byteIndex = 0U; byteIndex < length; byteIndex++) { // Workaround Part 1: Disable the global interrupts INTERRUPT_GlobalInterruptHighDisable(); // ------------------------------------ uint8_t readByte = FLASH_Read((flash_address_t) (startAddress + byteIndex)); // Workaround Part 2: Re-enable GIE once completed INTERRUPT_GlobalInterruptHighEnable(); // ------------------------------------ *crcSeed ^= (uint32_t) readByte; for (uint8_t bit = 8U; bit > 0U; --bit) { if ((*crcSeed & 0x01U) != 0U) { *crcSeed = (*crcSeed >> 1U) ^ CRC_POLYNOMIAL; } else { *crcSeed >>= 1U; } } } *crcSeed ^= CRC_XorOut; }
- Issue:
M8BTL-3377
Issue Title:
Operating UART without a pull-up resistor on the RX pin may lead to unstable behavior
Issue Description:
There is unstable behavior with the UART peripheral when utilizing the pin re-entry mechanism at POR on a CNano Base Board for Click Boards (AC164162). We believe it is related to how the MCU and debugger are being powered when attached to a baseboard.
It was recently discovered that the root cause of this issue is related to the floating signal on the Rx pin. Utilizing a pull-up on an Rx line is suggested to prevent from the floating signal from triggering some condition on the UART peripheral.
Workaround:
The issue is avoided when a pull-up is configured on the Rx pin. Navigate to the Pins Tab, and enable the Pull-up option for the UART RX pin.
- Issue:
M8BTL-3325
Issue Title:
AVR DU/EB CNano Evaluation Boards fail to update with factory default settings
Issue Description:
The AVR DU and EB CNano devices have Device Configuration Protection enabled by default in the on-board debugger which prevents the correct BOOT fuse value from being programmed.
Note: This is not an issue with the library design or embedded code
Workaround:
To work around this:
- Install Python 3.
- Run the package
installation command from a command line interface with access to
Python:
pip install pydebuggerconfig
- First, run the read
command to check the device's configuration. Check to see that the
FUSE_PROTECTION bit in the TARGET_DEBUG_FEATURES register is
set.
pydebuggerconfig read
- Next, disable the Fuse
Configuration Protection by
running:
pydebuggerconfig replace -r TARGET_DEBUG_FEATURES=0x07
If that process yields no errors, then you have successfully disabled Fuse configuration protection in the on-board debugger.
If for any reason you need to re-enable the Fuse Configuration Protection you can issue the command:pydebuggerconfig restore
If you do this please remember that this command will only restore the factory settings of the debugger and will not reset your device's Fuse values. If you have changed a Fuse then that value will be held until the debugger protection is disabled once again and you reprogram the device.
- Issue:
M8PD-11070
Issue Title:
PIC18F-Q10 devices have an incorrect page size in the exported payload
Issue Description:
A page size of 128 (0x80) is exported by the NVM driver payload and to the MDFU Client for PIC18FxxQ10 devices which leads to an incorrect assignment to WRITE_BLOCK_SIZE in the
bootloader_configuration.tomlfile. This in turn results in an update failure. Instead, the NVM driver needs to export 256 (0x100) as per the PIC18FxxQ10 datasheets.Workaround:
To workaround this issue, assign the
WRITE_BLOCK_SIZEin thebootloader_configuration.tomlfile with a value of0x100. Once this value is changed, save the file and pass the updated configuration file as a parameter to the pyfwimagebuilder. - Issue:
M8BTL-4664
Issue Title:
Reset function after END_TRANSFER needs longer delays for PIC devices
Issue Description:
During internal testing, it was identified that certain PIC devices using I2C may experience a bus lockup after the END transfer command due to a missing device-specific delay in the firmware. This issue does not affect UART or SPI interfaces. Users may observe that, although the application runs after an update, pymdfu reports a failure following the END transfer. To resolve this, a delay (approximately 14ms, depending on clock settings) should be added and tested to ensure reliable operation.
Workaround:
To workaround this issue increase the delay for PIC devices to at least 14ms by updating the bold line below in theDeviceResetCheckfunction of thebl_ftp.cfile:static void DeviceResetCheck(void) { if (resetPending == true) { #if defined(PIC_ARCH) __delay_ms(10U); RESET(); #elif defined(AVR_ARCH) _delay_ms(10U); ccp_write_io((void *) &RSTCTRL.SWRR, RESET_BIT_MASK); #endif } }