16.4 Changing the Default Function Allocation
The assembly code associated with a C/C++ function can be placed at an
absolute address. This can be accomplished by using the address attribute
and specifying the virtual address of the function, see 8.11 Variable Attributes.
Functions can also be placed at specific positions by placing them in a user-defined section and then linking this section at an appropriate address, see 8.11 Variable Attributes.
-mpure-code option (see 5.7.1 Options Specific to PIC32C/SAM Devices). This option ensures
that text sections do not contain read-only data, which would be inaccessible if such data
was present in XOM, and places a special flag on text sections to indicate that they
contain purely code and no data. The use of XOM can help protect firmware from being stolen
or reverse engineered by third parties. For example, add the following to your linker
script.SECTIONS
{
.purecode :
{
INPUT_SECTION_FLAGS (SHF_ARM_PURECODE) *(.text .text.*)
} > purecode_memory
}This change will ensure that input sections whose name matches .text or
.text.* and which are marked with the SHF_ARM_PURCODE
section flag (set by the -mpure-code option), will be placed in the
.purecode output section. That .purecode output
section will be mapped to a memory region named purecode_memory, which
must have previously been defined using the MEMORY command to associate it
with the desired XOM locations on your target device. For more information on linker
scripts, see the MPLAB XC32 Assembler, Linker, and Utilities User's Guide
(DS50002186).