4.4.2 xc32-as (32-bit Assembler)
A subset of command-line options may be specified in MPLAB X IDE. Select a category, and then set up assembler options. For additional options, see MPLAB XC32 Assembler documentation. See also “4.4.7 Options Page Features”.
| Option | Description | Command Line |
|---|---|---|
| Have symbols in production build | Generate debugging information for source-level debugging in MPLAB X. | --gdwarf-2 |
| Keep local symbols | Check to keep local symbols, i.e., labels beginning with .L (upper case only). Uncheck to discard local symbols. | --keep-localsSee MPLAB® XC32 Assembler, Linker and Utilities User's Guide. |
| Preprocessor macro definitions | Project-specific preprocessor macro defines passed via the compiler's –D option. |
|
| Assembler symbols | Define symbol 'sym' to a given 'value'. | --defsym sym=valueSee MPLAB® XC32 Assembler, Linker and Utilities User's Guide. |
| Preprocessor Include directories | Relative paths are from MPLAB X project directory. |
|
| Assembler Include directories | Relative paths are from MPLAB X project directory. Add a directory to the list of directories the assembler searches for files specified in You may add as many directories as necessary to include a variety of paths. The current working directory is always searched first and then | -I dirSee MPLAB® XC32 Assembler, Linker and Utilities User's Guide. |
| Option | Description | Command Line |
|---|---|---|
| Diagnostics level | Select warnings to display in the Output window. Select “Generate warnings” to have the usual warnings issued by the compiler; “Suppress warnings”to have only errors displayed, and "Fatal Warnings" to have the assembler treat warnings as if they were errors. | --[no-]warn
|
| Include source code | Check for a high-level language listing. High-level listings require that the assembly source code is generated by a compiler, a debugging option like -g is given to the compiler, and assembly listings (-al) are requested.Uncheck for a regular listing. | -ahSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Expand macros | Check to expand macros in a listing. Uncheck to collapse macros. | -amSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Include false conditionals | Check to include false conditionals (.if, .ifdef) in a listing.Uncheck to omit false conditionals. | -acSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Omit forms processing | Check to turn off all forms processing that would be performed by the listing directives .psize, .eject, .title and .sbttl.Uncheck to process by listing directives. | -anSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Include assembly | Check for an assembly listing. This -a suboption may be used with other suboptions.Uncheck to exclude an assembly listing. | -alSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| List symbols | Check for a symbol table listing. Uncheck to exclude the symbol table from the listing. | -asSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Omit debugging directives | Check to omit debugging directives from a listing. This can make the listing cleaner. Uncheck to included debugging directives. | -adSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| List to file | Use this option if you want the assembly listing for any assembly source files in the project. They will have the same basename as the source, with a | -a=file.lstSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |