5.1.2 Environment Variables
The variables in this section are optional, but, if defined, they will be used by the compiler. The compiler driver, or other subprogram, may choose to determine an appropriate value for some of the following environment variables if they are not set. The driver, or other subprogram, takes advantage of internal knowledge about the installation of the compiler. As long as the installation structure remains intact, with all subdirectories and executables remaining in the same relative position, the driver or subprogram will be able to determine a usable value. The “XC32” variables should be used for new projects; however, the “PIC32” variables may be used for legacy projects.
| Option | Definition |
|---|---|
XC32_C_INCLUDE_PATH
|
This variable’s value is a
semicolon-separated list of directories, much like PATH. When
the compiler searches for header files, it tries the directories listed in the
variable, after the directories specified with -I but before
the standard header file directories.If the environment variable is undefined, the preprocessor chooses an appropriate value based on the standard installation. By default, the following directories are searched for include files:
|
XC32_COMPILER_PATH
|
The value of
XC32_COMPILER_PATH is a semicolon-separated list of
directories, much like PATH. The compiler tries the
directories thus specified when searching for subprograms, if it can’t find the
subprograms using XC32_EXEC_PREFIX. |
XC32_EXEC_PREFIX
|
If XC32_EXEC_PREFIX is set,
it specifies a prefix to use in the names of subprograms executed by the
compiler. No directory delimiter is added when this prefix is combined with the
name of a subprogram, but you can specify a prefix that ends with a slash if
you wish. If the compiler cannot find the subprogram using the specified
prefix, it tries looking in your PATH environment variable.If the Other prefixes specified
with the Under normal circumstances it is best to leave this value undefined and let the driver locate subprograms itself. |
XC32_LIBRARY_PATH
|
This variable’s value is a
semicolon-separated list of directories, much like PATH. This
variable specifies a list of directories to be passed to the linker. The
driver’s default evaluation of this variable is:
|
TMPDIR |
If TMPDIR is set, it
specifies the directory to use for temporary files. The compiler uses temporary
files to hold the output of one stage of compilation that is to be used as
input to the next stage: for example, the output of the preprocessor, which is
the input to the compiler proper. |