5.7.8.5 Imacros Option
The -imacros file option processes the specified
file in the same way the -include option would, except that any output
produced by scanning the file is thrown away. The macros that the file defines remain
defined during processing. Because the output generated from the file is discarded, the
only effect of this option is to make the macros defined in file available for use in
the main input.
Any -D and -U options on the command
line are always processed before an -imacros option, regardless of the
order in which they are placed. All the -include and
-imacros options are processed in the order in which they are
written.