3.3.5.3 How Do I Make a Function Inline?
The XC32 compiler does not inline any functions when not optimizing.
By declaring a function inline, you can direct the XC32 compiler to make calls to that function faster. One way XC32 can achieve this is to integrate that function's code into the code for its callers. This makes execution faster by eliminating the function-call overhead; in addition, if any of the actual argument values are constant, their known values may permit simplifications at compile time so that not all of the inline function's code needs to be included. The effect on code size is less predictable; object code may be larger or smaller with function inlining, depending on the particular case.
To declare a function inline, use the inline keyword in its declaration, like this:
static inline int
inc (int *a)
{
return (*a)++;
}
For a function qualified both inline
and static
, if all calls to the function are integrated into the caller and the function's address is never used, then the function's own assembler code is never referenced. In this case, XC32 does not actually output assembler code for the function. Some calls cannot be integrated for various reasons (in particular, calls that precede the function's definition cannot be integrated, and neither can recursive calls within the definition). If there is a non-integrated call, then the function is compiled to assembler code as usual. The function must also be compiled as usual if the program refers to its address, because that can't be inlined. Enable optimization level -O1
or greater to enable function inlining.