5.1.1 Driver Command-line Format

The compilation driver program (xc32-gcc) compiles, assembles and links C and assembly language modules and library archives. The xc32-g++ driver must be used when the module source is written in C++. Most of the compiler command line options are common to all implementations of the GCC toolset; a few are specific to the compiler.

The basic form of the compiler command line is:
xc32-gcc [options] files libraries
xc32-g++ [options] files libraries
For example, to compile, assemble and link the C source file hello.c, creating the executable file hello.elf,execute this command:
xc32-gcc -o hello.elf hello.c
Or, to compile, assemble and link the C++ source file hello.cpp, creating the executable file hello.elf, execute:
xc32-g++ -o hello.elf hello.cpp

The available options are described in Driver Option Descriptions. It is conventional to supply options (identified by a leading dash “-” before the filenames), although this is not mandatory.

The files may be any mixture of C/C++ and assembler source files, relocatable object files (.o) or archive files. The order of the files is important. It may affect the order in which code or data appears in memory or the search order for symbols. Typically archive files are specified after source files. The file types are described in Input File Types.

Note: Command line options and file names are case sensitive.

The libraries is a list of user-defined object code library files that will be searched by the linker, in addition to the standard C libraries. The order of these files will determine the order in which they are searched. They are typically placed after the source filenames, but this is not mandatory.

It is assumed in this manual that the compiler applications are either in the console’s search path, the appropriate environment variables have been specified, or the full path is specified when executing any application.