13.6 Has_builtin Operator

The __has_builtin operator evaluates to a constant integer that can be used in integer contexts, such as the conditional expressions to the #if and #elif preprocessor directives, to test whether the compiler recognizes the operator's argument as the name of a built-in function in the current language and conformance mode. A nonzero value is yielded if the argument is a recognized built-in function; zero otherwise.

The __has_builtin operator by itself, without any operand or parentheses, acts like a predefined macro, so that code can test for its validity in a portable way. For example:
#if defined __has_builtin
#  if __has_builtin (__builtin_object_size)
#    define builtin_object_size(ptr) __builtin_object_size (ptr, 2)
#  endif
#endif
#ifndef builtin_object_size
#  define builtin_object_size(ptr)   ((size_t)-1)
#endif