1.2 LED Shadow Client Application
This example application shows how to use the shadow client feature to set/get Device status using LED(s). The device turns LED ON/OFF once to indicate the Shadow state is ready following which the user may turn LED(s) ON/OFF from AWS console. The application uses ECC608 for key storage and authentication.
Development Kits
The following table provides links to documentation on how to build and run LED Shadow Client Application on different development kits: