1 Approval Information

Table 1-1. Regulatory Approval Information
Country Regulatory Agency / Reference Approval Number Regulatory Information (Module) Regulatory Information (End Product)
Algeria ARPT 431/IR/HMG/PC/ARPCE/2022

Trademark:

Microchip Technology Inc.

Model:

ATWILC3000-MR110CA

Serial Number:

MAC Address on module label

CE Marking:

Available on module

“Made in” remark available on module packaging label

N/A
Argentina ENACOM RAMATEL Registration Number: C-17719

The external label must be composed of the module RAMATEL registration number, preceded by the legend “CONTAINS”, using one of the following models:

Armenia PSRC AST-016/S.A-0275-2021 Follows CE Follows CE
Aruba DOT DTZ/233/2017/IZ N/A N/A
Australia ACMA N/A
Follow ACMA guidelines for end product.
Azerbaijan RS AZ 031.55.02.01991.22 Follows CE Follows CE
Bahamas URCA URCA_TA_2017_003 Follow FCC Follow FCC
Bahrain TRA DLM/1416/10775 Follow CE Follow CE
Belarus MCI BY/112 10.3.1Д 020 00760
N/A
Benin ATRPT 2022-078/ARCEP/SE/DJPC/DAR/GU Follow CE Follow CE
Bolivia ATT ATT-DJ-RA-H-TL LP 136/2017 N/A N/A
Botswana BOCRA BOCRA/TA/2020/3216

BTA REGISTERED No.:

BOCRA/TA/2020/3216

BTA REGISTERED No.:

BOCRA/TA/2020/3216

Label must have a minimum height of 2 mm. Follow BOCRA guidelines for end product.

Brazil ANATEL ANATEL: 01424-17-03464

  1. ANATEL number must be placed on the end product.
  2. The final host device will include the sentence “este product contém a placa ATWILC3000-MR110CA código de homologação ANATEL 01424-17-03464” in the user's manual.
Cambodia MPTC 0014-2017-10CA N/A N/A
Cameroon ART 00000357/ART/DG/DT/SDNA/SNH/CA1 Follow CE Follow CE
Canada ISED 20266-ATWILC3000

IC: 20266-ATWILC3000

HVIN: ATWILC3000-MR110CA

Exterior label should use wording such as the following or similar:

Contains IC: 20266-ATWILC3000

Chile SUBTEL 5268/DO N° 38004/F26 5268/DO N° 38004/F26 (Voluntary)

5268/DO N° 38004/F26 (Voluntary)

Place the label on the end product (Voluntary)

China SRRC CMIIT ID: 2016DJ2596 CMIIT ID: 2016DJ2596

The end product also needs to show

本设备包含型号核准代码为: CMIIT ID:

2016DJ2596 的无线电发射模块 on the product label.

Columbia CRC 2017801086 N/A N/A
Congo ARPTC HIR – 0024/2017 N/A N/A
Costa Rica SUTEL 01496-SUTEL-DGC-2017 N/A N/A
Cote D'ivore ARTCI 064/DG/DRCT/DCO/SHO/KKC Follow CE Follow CE

Dominican

Republic

INDOTEL DE-0001297-17 N/A N/A
Ecuador ARCOTEL ARCOTEL-2017-003635 Follow FCC Follow FCC
Egypt NTRA TAC.14021714269.WIR N/A N/A
EU CE CE
Follow European guidelines.
Fiji TAF FJ17/31WL/11392 N/A N/A
Ghana NCA 1R3-1M-7E1-x09 NCA APPROVED:1R3-1M-7E1-x09

NCA APPROVED:1R3-1M-7E1-x09

Follow NCA guidelines for end product.

Grenada NTRC CL 1080 / 17 - TA N/A N/A
Honduras CONATEL 1481/2017 N/A N/A
India ETA NR-ETA/5647-RLO(NR) N/A N/A
Israel MOC 55-12055 MOC cert. no.: 55-12055

End product's ID.

Place the label on the end product.

Jamaica SMA N/A N/A

This product contains a Type Approved Module

by Jamaica: SMA - ATWILC3000-MR110CA

Japan MIC 005-101536

Contains Transmitter Module

The diameter of Japan Approved Mark must be min. > 3 mm.

Jordan TRC TRC/11/11554/2023

(Voluntary)

Place the label on the end product (Voluntary).

Follow TRC guidelines.

Kenya CA CA/LCS/1600/00316/Vol.1 N/A N/A
Kuwait CITRA 4778 N/A N/A
Lebanon TRA 3840/E&M/2017 N/A N/A
Lesotho LCA LCA/TA/72/2017 N/A N/A
Madagascar ARTEC 16/195/ARTEC/DG/DHCT/SSS/test N/A N/A
Malawi MACRA 504 N/A N/A
Mauritius ICTA TA/2017/0238 N/A N/A
Mexico IFT RTIATAT17-0485

IFT: RTIATAT17-0485

La operación de este equipo está sujeta a las siguientes dos condiciones: (1) es posible que este equipo o dispositivo no cause interferencia perjudicial y (2) este equipo o dispositivo debe aceptar cualquier interferencia, incluyendo la que pueda causar su operación no deseada.

Label can be put the manual or packaging

RTIATAT17-0485

La operación de este equipo está sujeta a las siguientes dos condiciones: (1) es posible que este equipo o dispositivo no cause interferencia perjudicial y (2) este equipo o dispositivo debe aceptar cualquier interferencia, incluyendo la que pueda causar su operación no deseada.

Place the label on the end product.

Moldova ANCERTI MD OC TIP 024 CET7346-21
Morocco ANRT MR 13272 ANRT 2017
Mozambique INCM 1/R/MCL/2017 N/A N/A
Namibia CRAN TA - 2016/1400 N/A N/A
Nepal NTA R-SRD-PP-553 N/A N/A
New Zealand RSM N/A R-NZ Follow RSM guidelines for end product
Nicaragua TELCOR NCG-CE-17-026 N/A N/A
Nigeria NCC NCC/TSNI/WN/TA/CERT/1481/2017

Label can be put on the manual or packaging.

Follow NCC guidelines for the end product.

Oman TRA TRA/TA-R/3940/17

Label can be put on the manual or packaging.

Follow TRA guidelines for end product.
Pakistan PTA 9.073/2017

Follow PTA guidelines for end product.

Panama ASEP 1825 N/A N/A

Papua New

Guinea

NICTA PNG17/0988 N/A N/A
Paraguay CONATEL 2022-05-I-0300

Place the label on the end product.

Peru MTC 1700010 N/A N/A
Qatar ICT CRA/SA/2017/R-5994 N/A N/A
Russia FCA

In Russia: МДРД-6620

In English: MDRD-6620

N/A N/A
Saudi Arabia CITC 2023-87 N/A N/A
Senegal ARTP 070816/AG/ER N/A N/A
Singapore IMDA N0088-22
South Africa ICASA TA-2016/3408

Label can be put on the manual or packaging.

  1. Update as per ICASA label dimension letter to Microchip.
  2. Follow ICASA guidelines.
South Korea RRA MSIP-CRM-mcp-WILC3000MR110C

Follow RRA guidelines for end product.

Swaziland SCCOM TA-2017/0005 N/A N/A
Taiwan NCC CCAJ16LP4160T4

Label can be put on the manual or packaging.

Label must be on the product. No size requirement, but it needs to be clearly visible.

This exterior label can use wording such as the following:

Contains Transmitter Module:

or similar wording.

Tanzania TCRA TCRA/TAC/016/2017 N/A N/A
Thailand NBTC N/A N/A N/A
Tunisia CERT AHO-1843-21 N/A N/A

UAE

(United Arab Emirates)

TRA ER51920/17

Label can be put on the manual or packaging.

End product’s TRA certification number and Dealer’s number.

Follow TRA guidelines for the end product.

Uganda UCC N/A N/A N/A
Ukraine UkrSEPRO UA.TR.001.0355.30.00896-21
Place the label on the end product.
Uruguay URSEC 742/DAE/2016 N/A N/A
USA FCC 2ADHKWILC3000 FCC ID: 2ADHKWILC3000

The outside of final products that contains this module device must display a label referring to the enclosed module. This exterior label can use wording such as the following:

FCC ID: 2ADHKWILC3000

or

Contains FCC ID:2ADHKWILC3000

Venezuela CONATEL N/A N/A N/A
Vietnam MIC C1041170921AE01A3
The end product requires its own certification.

The label will show the information related to the end product certification. However, the end product label does not need to show the module information.

Zambia ZICTA ZMB/ZICTA/TA/2017/3/40
Zimbabwe POTRAZ POZ514 N/A N/A
Note: N/A = Not Applicable