1 Approval Information
| Country | Regulatory Agency / Reference | Approval Number | Regulatory Information (Module) | Regulatory Information (End Product) |
|---|---|---|---|---|
| Algeria | ARPT | 431/IR/HMG/PC/ARPCE/2022 |
Trademark: Microchip Technology Inc. Model: ATWILC3000-MR110CA Serial Number: MAC Address on module label CE Marking: Available on module “Made in” remark available on module packaging label | N/A |
| Argentina | ENACOM | RAMATEL Registration Number: C-17719 |
The external label must be composed of the module RAMATEL registration number, preceded by the legend “CONTAINS”, using one of the following models: | |
| Armenia | PSRC | AST-016/S.A-0253-2024 | Follows CE | Follows CE |
| Aruba | DOT | DTZ/233/2017/IZ | N/A | N/A |
| Australia | ACMA | N/A | Follow ACMA guidelines for end product. | |
| Azerbaijan | RS | AZ 031.30.02.03560.24 | Follows CE | Follows CE |
| Bahamas | URCA | URCA_TA_2017_003 | Follow FCC | Follow FCC |
| Bahrain | TRA | DLM/1416/10775 | Follow CE | Follow CE |
| Belarus | MCI | BY/112 10.3.1Д 020 00760 | N/A | |
| Benin | ATRPT | 2022-078/ARCEP/SE/DJPC/DAR/GU | Follow CE | Follow CE |
| Bolivia | ATT | ATT-DJ-RA-H-TL LP 136/2017 | N/A | N/A |
| Botswana | BOCRA | BOCRA/TA/2020/3216 |
BTA REGISTERED No.: BOCRA/TA/2020/3216 |
BTA REGISTERED No.: BOCRA/TA/2020/3216 Label must have a minimum height of 2 mm. Follow BOCRA guidelines for end product. |
| Brazil | ANATEL | ANATEL: 01424-17-03464 |
|
|
| Cambodia | MPTC | 0014-2017-10CA | N/A | N/A |
| Cameroon | ART | 00000357/ART/DG/DT/SDNA/SNH/CA1 | Follow CE | Follow CE |
| Canada | ISED | 20266-ATWILC3000 |
IC: 20266-ATWILC3000 HVIN: ATWILC3000-MR110CA |
Exterior label should use wording such as the following or similar: Contains IC: 20266-ATWILC3000 |
| Chile | SUBTEL | 5268/DO N° 38004/F26 | 5268/DO N° 38004/F26 (Voluntary) |
5268/DO N° 38004/F26 (Voluntary) Place the label on the end product (Voluntary) |
| China | SRRC | CMIIT ID: 2016DJ2596 | CMIIT ID: 2016DJ2596 |
The end product also needs to show 本设备包含型号核准代码为: CMIIT ID: 2016DJ2596 的无线电发射模块 on the product label. |
| Columbia | CRC | 2017801086 | N/A | N/A |
| Congo | ARPTC | HIR – 0024/2017 | N/A | N/A |
| Costa Rica | SUTEL | 01496-SUTEL-DGC-2017 | N/A | N/A |
| Cote D'ivore | ARTCI | 064/DG/DRCT/DCO/SHO/KKC | Follow CE | Follow CE |
|
Dominican Republic | INDOTEL | DE-0001297-17 | N/A | N/A |
| Ecuador | ARCOTEL | ARCOTEL-2017-003635 | Follow FCC | Follow FCC |
| Egypt | NTRA | TAC.14021714269.WIR | N/A | N/A |
| EU | CE | CE | Follow European guidelines. | |
| Fiji | TAF | FJ17/31WL/11392 | N/A | N/A |
| Ghana | NCA | 1R3-1M-7E1-x09 | NCA APPROVED:1R3-1M-7E1-x09 |
NCA APPROVED:1R3-1M-7E1-x09 Follow NCA guidelines for end product. |
| Grenada | NTRC | CL 1080 / 17 - TA | N/A | N/A |
| Honduras | CONATEL | 1481/2017 | N/A | N/A |
| India | ETA | NR-ETA/5647-RLO(NR) | N/A | N/A |
| Israel | MOC | 55-12055 | MOC cert. no.: 55-12055 |
End product's ID. Place the label on the end product. |
| Jamaica | SMA | N/A | N/A |
This product contains a Type Approved Module by Jamaica: SMA - ATWILC3000-MR110CA |
| Japan | MIC | 005-101536 |
|
Contains Transmitter Module The diameter of Japan Approved Mark must be min. > 3 mm. |
| Jordan | TRC | TRC/11/11554/2023 | (Voluntary) |
Place the label on the end product (Voluntary). Follow TRC guidelines. |
| Kenya | CA | CA/LCS/1600/00316/Vol.1 | N/A | N/A |
| Kuwait | CITRA | 4778 | N/A | N/A |
| Lebanon | TRA | 3840/E&M/2017 | N/A | N/A |
| Lesotho | LCA | LCA/TA/72/2017 | N/A | N/A |
| Madagascar | ARTEC | 16/195/ARTEC/DG/DHCT/SSS/test | N/A | N/A |
| Malawi | MACRA | 504 | N/A | N/A |
| Mauritius | ICTA | TA/2017/0238 | N/A | N/A |
| Mexico | IFT | RTIATAT17-0485 |
IFT: RTIATAT17-0485 La operación de este equipo está sujeta a las siguientes dos condiciones: (1) es posible que este equipo o dispositivo no cause interferencia perjudicial y (2) este equipo o dispositivo debe aceptar cualquier interferencia, incluyendo la que pueda causar su operación no deseada. Label can be put the manual or packaging |
RTIATAT17-0485 La operación de este equipo está sujeta a las siguientes dos condiciones: (1) es posible que este equipo o dispositivo no cause interferencia perjudicial y (2) este equipo o dispositivo debe aceptar cualquier interferencia, incluyendo la que pueda causar su operación no deseada. Place the label on the end product. |
| Moldova | ANCERTI | MD OC TIP 024 CET7346-21 | ||
| Morocco | ANRT | MR 13272 ANRT 2017 | ||
| Mozambique | INCM | 1/R/MCL/2017 | N/A | N/A |
| Namibia | CRAN | TA - 2016/1400 | N/A | N/A |
| Nepal | NTA | R-SRD-PP-553 | N/A | N/A |
| New Zealand | RSM | N/A | R-NZ | Follow RSM guidelines for end product |
| Nicaragua | TELCOR | NCG-CE-17-026 | N/A | N/A |
| Nigeria | NCC | NCC/TSNI/WN/TA/CERT/1481/2017 |
Label can be put on the manual or packaging. |
Follow NCC guidelines for the end product. |
| Oman | TRA | TRA/TA-R/3940/17 |
Label can be put on the manual or packaging. | Follow TRA guidelines for end product. |
| Pakistan | PTA | 9.073/2017 | Follow PTA guidelines for end product. | |
| Panama | ASEP | 1825 | N/A | N/A |
|
Papua New Guinea | NICTA | PNG17/0988 | N/A | N/A |
| Paraguay | CONATEL | 2022-05-I-0300 |
![]() | ![]() Place the label on the end product. |
| Peru | MTC | 1700010 | N/A | N/A |
| Qatar | ICT | CRA/SA/2017/R-5994 | N/A | N/A |
| Russia | FCA |
In Russia: МДРД-6620 In English: MDRD-6620 | N/A | N/A |
| Saudi Arabia | CITC | 2023-87 | N/A | N/A |
| Senegal | ARTP | 070816/AG/ER | N/A | N/A |
| Singapore | IMDA | N0088-22 | ||
| South Africa | ICASA | TA-2016/3408 | Label can be put on the manual or packaging. |
|
| South Korea | RRA | MSIP-CRM-mcp-WILC3000MR110C | Follow RRA guidelines for end product. | |
| Swaziland | SCCOM | TA-2017/0005 | N/A | N/A |
| Taiwan | NCC | CCAJ16LP4160T4 |
|
Label must be on the product. No size requirement, but it needs to be clearly visible. This exterior label can use wording such as the following: Contains Transmitter Module: or similar wording. |
| Tanzania | TCRA | TCRA/TAC/016/2017 | N/A | N/A |
| Thailand | NBTC | N/A | N/A | N/A |
| Tunisia | CERT | AHO-1843-21 | N/A | N/A |
|
UAE (United Arab Emirates) | TRA | ER51920/17 |
Label can be put on the manual or packaging. |
End product’s TRA certification number and Dealer’s number. Follow TRA guidelines for the end product. |
| Uganda | UCC | N/A | N/A | N/A |
| Ukraine | UkrSEPRO | UA.TR.001.0355.30.00896-21 | Place the label on the end product. | |
| Uruguay | URSEC | 742/DAE/2016 | N/A | N/A |
| USA | FCC | 2ADHKWILC3000 | FCC ID: 2ADHKWILC3000 |
The outside of final products that contains this module device must display a label referring to the enclosed module. This exterior label can use wording such as the following: FCC ID: 2ADHKWILC3000 or Contains FCC ID:2ADHKWILC3000 |
| Venezuela | CONATEL | N/A | N/A | N/A |
| Vietnam | MIC | C0609130924AE01A3 (COO:Thailand) | The end product requires its own certification. The label shows the information related to the end product certification. However, the end product label does not need to show the module information. | |
| C0548040924AE01A3(COO:China) | ||||
| Zambia | ZICTA | ZMB/ZICTA/TA/2017/3/40 | ||
| Zimbabwe | POTRAZ | POZ514 | N/A | N/A |