1.11 NVMCTRL Read Write

This example application demonstrates how to use the NVMCTRL to erase and program the internal Flash memory.

Description

This example uses the NVMCTRL peripheral library to erase a row and write an array of values to the internal Flash memory. It verifies the value written by reading the values back and comparing it to the value written.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/nvmctrl/nvmctrl_flash_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_ha1_xpro.XMPLABX project for SAM HA1G16A Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_ha1_xpro.XSAM HA1G16A Xplained Pro Evaluation Kit

Setting Up SAM HA1G16A Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable
Note: ATSAMHA1G16A device in SAM HA1G16A Xplained Pro board is not recommended for new design, hence replace the device with ATSAMHA1G16AB device. Connect the supported external debugger to Cortex Debug Port.

Running the Application

  1. Build and Program the application using its IDE
  2. The LED indicates the success or failure:
    • LED is turned ON when the value read from the flash memory matched with the written value
    • LED is turned OFF when the value read from the flash memory did not match with the written value
  3. The following table provides the LED name: