10.3.1.1.1 Physical Sections
The Flash is divided physically into two fixed sections: A Read-While-Write (RWW) section and a No-Read-While-Write (NRWW) section.
The main differences between the two sections are as follows:
- When erasing or writing a page located inside the RWW Flash, the NRWW Flash can be read during the operation
- When erasing or writing a page located inside the NRWW Flash, the CPU is halted during the entire operation
The syntax “Read-While-Write section” refers to which section to program (erase or write), not the one read. Only the code located inside the NRWW Flash is accessible by either executing a CPU instruction or reading data while the RWW Flash is being written or erased.
Note: The interrupt code in the RWW section may
halt the CPU if the associated interrupt is triggered while the RWW section is erased or
written. Disable or place the interrupt code in the Boot Code (BOOT) section to avoid
this.
The figures and table below explain these two physical Flash sections in detail:
| Flash Section Erased/Written | Flash Section Accessed | CPU |
|---|---|---|
| RWW section | NRWW section | Running |
| NRWW section | NRWW section | Halted |
| RWW section | RWW section | Halted |
Note:
- The User Row is located in the RWW Flash. When erasing or writing a page in the User Row, the NRWW Flash can be read during the operation.
- The Boot Row is located in the RWW Flash. When erasing or writing a page in the Boot Row, the NRWW Flash can be read during the operation.
- The physical section sizes are device-dependent. Refer to the Memory Overview section for further details.