1 Harmony 3 Driver, System Services and RTOS Application Examples for PIC32CK GC/SG Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers,system services and RTOS.
Name | Description |
---|---|
Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
FAT File System using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
FAT File System using SD Card media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
FAT File System using SDMMC Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDMMC driver |
FAT File System using SST26 Media | This application shows an example of using the FAT File System to access SQI based SST26 flash media |
FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
I2C Driver Asynchronous - Multi-client | This example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
SPI EEPROM AT25 Driver - EEPROM Read Write | This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
TrustZone FreeRTOS Basic | This example application blinks an LED to show the FreeRTOS threads that are running in non-secure mode and to indicate status |
USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |