1 Harmony 3 Driver, System Services and RTOS Application Examples for PIC32CK GC/SG Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers,system services and RTOS.
| Name | Description |
|---|---|
| Console Debug System Service Using UART | This example application demonstrates the UART based console and debug system service |
| FAT File System Using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT File System Using SD Card Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of an SD card using the SDSPI driver and the SPI PLIB |
| FAT File System Using SDMMC Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of an SD card using the SDMMC driver |
| FAT File System Using SST26 Media | This application shows an example of using the FAT File System to access SQI based SST26 Flash media |
| SFDP Flash Driver - Flash Read Write in Quad IO Mode | This example application shows how to use the SFDP Flash driver to perform block operations on JEDEC-compliant NOR Flash memory in SQI mode. |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
| I2C Driver Asynchronous - Multi Client | This example application demonstrates the multi-client feature of the Asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
| SPI Driver Asynchronous - Self-Loopback Multi Client | This example demonstrates how to use the SPI driver in Asynchronous mode to achieve self-loopback between multiple clients |
| SPI Driver Synchronous - Self-Loopback Multi Client | This example demonstrates how to use the SPI driver in Synchronous mode to achieve self-loopback between multiple clients in RTOS environment |
| SPI EEPROM AT25 Driver - EEPROM Read Write | This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
| Time System Service Multi Client | This example application demonstrates the multi-client system timer functionality |
| TrustZone® FreeRTOS Basic | This example application blinks an LED to show the FreeRTOS threads that are running in Non-Secure mode and to indicate status |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in Asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in Synchronous mode |