2.4.3.6 OTA Control Point Behavior

The OTA Control Point is used by a Client to control certain behaviors of the Server.

The procedures are triggered by writing a value that includes an Opcode specifying the operation and this may be followed by a Parameter that is valid within the context of that Opcode . For each of the procedures described in the next sections, the Server shall indicate the OTACP characteristic with the Response Code Opcode (0x01) along with the Request Opcode and “Success” or other appropriate Result Code contained in the response as listed in Table 4.2.